The application is to mux an SD Card interface between two different processors using SN74CB3Q3257RGYR. The max clock speed will run at 33MHz. Wondering what is the impact of running the high-speed clock/data through the mux, I was thinking specifically in terms of SI. From what I understand the mux will be just a small resistance on the line (Rds ON) but was wondering if just by having to go through the device you could get impedance discontinuities and potential to impact the signals integrity.
The device lists USB as a possible applications but I just wanted to make sure it can handle high speed data rate without impacting SI and if there is any special considerations I need to take to make sure.
Thanks,
Alejandro