Other Parts Discussed in Thread: TS5A12301E, TS5A6542
Hello,
I was looking at using the SN74LVC1G66 instead of a load switch to shut off power because my application only pulls 10mA of power and I saw this device can handle up to 100mA MAX.
However, upon further inspection, I noticed that if I use a VCC of 3V, my Vlogic of 1.8V is below the Vcc*0.7 for VIH.
Can you suggest a device which will allow me to use the 3V Vcc/VIO, but control it using 1.8V logic?
Thanks,
Louie