Dear Sirs,
My customer asked us about PD pin of TS3L501E.
Is there a problem if the PD terminal is set to HIGH under the following conditions?
1.VDD=0V、Vin=0V(That is, in a state where a voltage of HIGH is applied only to the PD pin.)2.VDD=0V、Vin>0V We have confirmed that this condition is prescribed in the specification of Ioff on page 6 of the datasheet. I also confirmed the following contents of E2E. Here "Vin = 0 to 3.6 V" is typo.Is Vin = 3.6 V correct? Please let me know about the above contents.Best Regards,Y. Hasebe