This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need Help in selecting a part

Other Parts Discussed in Thread: TLV271, TMUX1072, TS12A12511

Hi,

Need to select a SPDT multiplexer which would select one of the inputs and connect to the output based on the select inputs of the multiplexer

Input 1 : A sense signal ( Output of a TLV271 opamp)

Input 2 : A sense signal ( Output of a TLV271 opamp)

Based on the select signal (0 or 1) I need one of the inputs to be relayed to the output pin of the multiplexer.

Requirements:

Bandwidth > 10MHz ( To make sure that the relayed signal does not have any phase lag introduced).

Resistance of the path < 10E

Current carrying capability of the switch : < 10mA (Ok, even if its more)

Supply voltage: 5V and 12V( Two different cases)

Regards,

Rajesh Sura