This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD4051B: MUX/DEMUX LIN bus

Part Number: CD4051B
Other Parts Discussed in Thread: SN74CBT3251, TLIN2029-Q1, MUX508

Hello,

I would like to multiplex 5 LIN slave to my master (those slaves can't be on the same LIN bus).

I selected a TI transceiver from UART : TL2029.

I think that a CD4051B could work because Vdd can be up to 20V (that would eliminate a sn74cbt3251).

Is there any EVM available with this chip and/or would recommend another chip ?

Thanks