Other Parts Discussed in Thread: SN74CB3Q3125
Greetings,
I am using a TS3A4751PWR analog switch in the following generalized application which optionally turns on/off a 3.3k pull-up on a net.
The problem is that I have no control over when 3.3V_Remote turns on relative to the 3.3V (VCC) and there is a requirement in the datasheet that VCOM < VCC+0.3V. I'm looking for a solution that minimizes the changes to the design as much as possible. We were considering a) moving the 3.3k resistor to the COM input to reduce current or b) powering VCC through a 10k resistor, again to reduce current back onto the 3.3V rail. Without knowing the internal architecture of the device, it's difficult to determine whether either of our proposed solutions will work.
Thoughts?
Thank