This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS12A44514: TS12A44514 - the consumption current of Vcc

Part Number: TS12A44514

I want to drive the input controls using a DIO. How much current draw will each input require for a High and a Low?

  • Victor,

    The TS12A44514 like all the TI passive FET switches do not have a drive capability.  The logic high and low of the signal path will be determined by the transmitter and receiver you connect to the passive FET switch I/O pins COM and NO pins.  

    The current consumption Icc for the TS12A44154 is 50nA and it doesn't matter the voltage place on the I/O signal path.

    The digital control logic pins labeled "IN" for the TS12A44514 device are Hi-Z inputs and do not require large current to provide the switch with logic high or logic low.  It will only leak a couple of nA worst case.

    If you are looking for a device that has drive capability I would look at an I/O expander or a level shifter and not a FET switch.

    Thank you,

    Adam