Other Parts Discussed in Thread: PCA9515A
Hi,
For the Part SN74CBTLV3126 the datasheet specifies that the device supports Partial-Power-Down-Mode (Ioff) and the device has isolation during power off.
Can you let me know what exactly it is meant by Partial-Power-Down-Mode and what conditions we need to maintain to achieve isolation during power off.
We are seeing the device conducting from input(A's) to output(B's) when no supply(Vcc) is available with OE pin which is pulled down via by 10Kohm on our custom Board. When inputs(A's) are at 3.3V we are seeing a voltage level of 1.4V on outputs(B's). As such overall aim is have perfect isolation during power off state. Please let me know your thoughts on the same.
Regards,
Kiran