Browse Topics
Amplifiers
Audio Amplifiers
High Speed Amplifiers
Precision Amplifiers
/etc... Amplifiers & Other Linear
Applications
Automotive
Medical & High Reliability
Motor Drivers
ARM® Processors
Sitara™ ARM®
Digital Signal Processors (DSP)
C5000 Ultra Low Power DSP
C6000 Multicore DSP
C6000 Single Core DSP
DaVinci™ Video Processors
OMAP™ Processors
Clocks & Timers
Data Converters
Audio Converters
High Speed Data Converters
Precision Data Converters
Video Converters
/etc... Data Converters
Development Tools
WEBENCH® Design Center
Code Composer Studio
TI C/C++ Compiler
DLP & MEMS
Embedded Software
Android
BIOS
Linux
Multimedia Software Codecs
StarterWare
WinCE
Interface
Consumer & Computing
Ethernet
Fiber Communication
High Speed Interface
Industrial Interface
/etc... Interface
Logic
Low Power RF & Wireless Connectivity
Microcontrollers
MSP430™ Microcontrollers
Stellaris® ARM® Microcontrollers
Tiva™ ARM® Microcontrollers
Other Microcontrollers
C2000™ Microcontrollers
Hercules™ Safety Microcontrollers
OMAP™ Applications Processors
Power Management
Battery Management
Digital Power
AC/DC and Isolated DC/DC Power
LED Drivers/LCD Bias
Linear Regulators
NexFET™ Power MOSFETs
Non-Isolated DC/DC
Power Modules
PMU
Power Interface
SIMPLE SWITCHER®
Sequencers
Supervisor and Reset IC
Wireless Power
/etc... Power
RF & Digital Radio
Digital Radio (GC Products)
High Performance RF Modulators, PLL and VCO products
/etc... RF
Other Analog & Touch
Imaging
Temperature Sensors
Touch
/etc... Analog
/etc Support
Custom Title
Support Forums
To post a question or find an answer, choose a topic from the "Browse Topics" navigation menu on the left.
Get this RSS feed
Tags
You have subscribed to this tag. To view or manage your tag subscriptions,
click here
.
Close
You have unsubscribed from this tag. To view or manage your tag subscriptions,
click here
.
Close
You are currently viewing:
AM3517
1271
1273
2.6.37
2.6.37 kernel
3530
6446
6467
Adeneo
am1808
AM1808 logicPD
am18x
am335x
am3505
am3505/17
AM3517 boot
AM3517 datasheet
AM3517 EVM
AM3517 EVM Linux
am3517 rowboat android
am3517 som
am35x
am35xx
am3715
AM37X
am37xx
Related Posts
Forum Post:
How are the Cortex-A8 based Sitara AM3505 and AM3517 optimized for the industrial market?
Phillip Parker
First ARM Cortex-A8 processor based solution optimized for industrial market, delivering greater ARM performance than previous alternatives in the market. Peripherals including CAN controller and Ethernet MAC as well as industrial temperature-grade options and package alternatives to enable developers...
on
Oct 20, 2009
Forum Post:
What is the roadmap for OMAP3503/3515 devices?
Phillip Parker
OMAP3503/15 - Sitara AM3505, AM3517 or AM Next generation devices depending on your needs. There will also be future ARM Cortex-A8 based products in the Sitara family that will offer higher performance and lower cost alternatives.
on
Oct 20, 2009
Forum Post:
multichannel audio application on 3517/05
Yan8622
On 3517/05 , are there enough I2S (or compatible) to handle 8-in/8-out audio channels, for example in a portable mixing console?
on
Nov 19, 2009
Forum Post:
AM3505 - USB3320 (Swap DP/DM) linux support
Christoph Gollinger
Dear Community Members, We want to connect a USB3320 USB transceiver to the USB2/ULPI Interface and want to use linux. There is a Swap DP/DM feature that can be accessed by setting the respective bit in the vendor specific register 0x39(write). We want to set it to 1 in order to prevent crossing DP...
on
Jan 7, 2010
Forum Post:
Using a Crystal with AM3517 (sys_xtalout and sys_xtalin pins)
Alex Milgrom
Hi All. I need information on the crystal that can be used on the sys_xtalout and sys_xtalin pins. The datasheet notes that a 26MHz Crystal or a 26MHz oscillator may be used here (defined by the sys_boot6 pin) but non of the reference designs I've seen uses a crystal (they all use an oscillator...
on
Jan 12, 2010
Forum Post:
AM3517: Recommended operating voltage specs
Mark Utter
The current AM3517 datasheet only specifies nominal recommended operating voltages for the device. Customer is in design and needs to know min and max for VDDCORE. The nominal VDDCORE is specified as 1.2V. They using the TPS65023. Due to a workaround, the VDDCORE comes up at 1.225V instead of 1.20V...
on
Jan 19, 2010
Forum Post:
AM3517 - Booting up time from Flash after bypasing USB and UART3
Pretesh Mascarenhas
Hi, I am planning to place the AM35XX in our design. I needed some infomation in regards to Boot up time as thats one of our requirement. The set up: I am not using the UART or USB boot options I need the CPU to boot up from the external NAND flash (GPMC) in normal operation. However...
on
Feb 9, 2010
Forum Post:
sys_clkreq pin ... a input or output ?
Pretesh Mascarenhas
Hi Say we are using an external CMOS digital clock through the sys_xtalin pin. In this case, the sys_clkreq is used as an output to request the external system clock. (1) Page 70 of datasheet – A CMOS digital clock through the sys_xtalin pin. In this case, the sys_clkreq is used as an output...
on
Feb 11, 2010
Forum Post:
AM3517 DDR2 memory Manhattan lentghs
miversen
Hi community, I have done Manhattan length calculations of a configuration with two DDR2 memories conected to AM3517. The AM3517 is placed at X,Y = 0,0 mm and the two DDR2 memories are placed at X,Yoffset = -44,+/-16 mm, which is the maximum allowable distance from AM3517 according to table 6-17 in the...
on
Feb 15, 2010
Forum Post:
Graphics frame rate with EGL
Tak Izaki
Hi, I have a trouble with frame rate of SGX530 graphics. I' now work on AM3517 EVM from LOGIC with Linux. I use SDK of Graphics. The frame rate of demo software seems 60Hz. I want to change the frame rate to 30 Hz. I believe eglSwapInterval() or PVRShellSet(prefSwapInterval, xx) can change...
on
Mar 17, 2010
Forum Post:
AM3517 EVM + Application board uboot issue
Diego Chaverri
Hi, I'm working with an AM3517 EVM Development Kit. I'm having trouble when connecting the Application board to the EVM, I get the following message: Texas Instruments X-Loader 1.45 (Mar 19 2010 - 19:44:22) Starting X-loader on MMC Reading boot sector 214940 Bytes Read from MMC Starting OS...
on
Apr 14, 2010
Forum Post:
real-time kernel patch
Dominique Holzwarth
hello is there a real-time kernel patch available for the kernel which is delivered with the PSP for the AM3517? currently i'm using the PSP 03.00.00.02 which has the kernel version 2.6.31-rc7. Update: The main reason why I have asked for a RT patch for the AM3517 PSP is because I've...
on
May 4, 2010
Forum Post:
AM3517 Video Capture Driver
Nhan Pham
HI, The current video capture driver doesn't support RGB input signal on the AM3517 application board. I wonder when will be one available for this input. Thanks Nhan Pham
on
May 10, 2010
Forum Post:
DDR2 Termination
fred50021
hi, is there an on-chip termination of the SDRC interface integrated in the am3505? in the am3505.pdf document on page 109 there are "T" symbols drawn on many lines. do they represent internal termination resistors and thus no additional termination is required (as always mentioned...
on
May 11, 2010
Forum Post:
USB ports speed
fred50021
hi, i am confused about the USB port speeds in the datasheets. It seams port0 ist the most comfortabel one to use. Can i use port0 as HS (480Mbps) host port for connecting USB Memory Sticks? thanks fred
on
May 12, 2010
Forum Post:
About difference of function on the N21 and N22 pin.
RY9983
Hello. We are one of the distributor of TI. Our customer is designing AM3517 system. Lately, new AM3517 datasheet was updated on TI web site. And, I found the functional difference of N21 and N22 pin in the new datasheet.(Table2-1, am3517.pdf) http://focus.ti.com/docs/prod/folders/print/am3517...
on
May 24, 2010
Forum Post:
Re: ALSA (ASoC) on AM3517 not working
Steve Preissig
Hi Ivan, I have been able to get the aplayer and arecord working with these settings. I am using: AM35x-OMAP35x-PSP-SDK-03.00.00.05.tar.gz arm-2009q1-203-arm-none-linux-gnueabi-i686-pc-linux-gnu.tar.bz2 I am running from the nfs filesystem (./images/filesystem/am3517/nfs.tar.gz) that comes...
on
Jun 25, 2010
Forum Post:
The problem about modversions of AM3517
hongbo dai
I am fresh to learm ARM. I insert a module to the kernel after I compiled it.But it failed. The error is like this: root@am3517-evm :~# insmod ./hello.ko hello: module_layout: kernel tainted. Disabling lock debugging due to kernel taint hello: version magic '2.6.32 mod_unload ARMv5 ' should...
on
Jul 17, 2010
Forum Post:
Unable to Read and write in External NAND[AM3517].
hrishikesh choudhary
Dear All, We have a custom board which has AM3517 controller interfaced to External NAND through FPGA. The Control signal and Data signal are routed through FPGA to NAND. Currently I am trying to Read ID from the NAND . But whatever value i write to the NAND in the form of Command is reflected back...
on
Apr 27, 2012
Forum Post:
u-boot splash screen image
hakan ��zcan
Hi everyone, I have am3517 based TAM3517 ( http://www.technexion.com/index.php/products/arm-cpu-modules/ti-sitara-am3517/tam-3517 ) and i want to add a splash screen image. I mean, i want to show some image while my device booting. since i am a newbie, is there anyway to do that ?
on
Apr 30, 2012
Forum Post:
State of SYS_NRESWARM after the reset
Daisuke Maeda
http://processors.wiki.ti.com/index.php/AM35x_Schematic_Checklist#RESETS I saw the following description in the above Wiki. 1. SYS_NRESWARM is pulled-low when SYS_NRESPWRON is LOW. 2. Once SYS_NRESPWRON goes HIGH, for PRM_RSTTIME, SYS_NRESWARM will be driven LOW (No pull down). 3. After that SYS_NRESWARM...
on
May 10, 2012
Forum Post:
TPS65920, POWER ON/OFF SEQUENCE
RAJEEV BATTU
Hi Team, I am new to omap world. I am working with AM3517. By using TPS65920 i want to implement safe shutdown/poweroff I went through datasheet and searched TI site, still i have some doubts about the work flow of TPS65920. The on/off sequence of entire system. PWR_ON, SYS_ENB pins functionality...
on
May 22, 2012
Forum Post:
Video can't be played on am3517 with android 2.3.4.
Kevin Chow
Hi, I am using am3517 with android 2.3.4, kernel 2.6.36, when play videos, eg. mp4, it will show as sequence pictures and it is very slow, even more it will stop and do nothing, why? below is my ddms log: --------------------------------------------- 01-01 02:08:34.312: E/InputDispatcher(1710...
on
Jul 9, 2012
Forum Post:
VDDS_DSI and AM3505 - Is there a need for a VDDS_DSI regulator?
Raphaël Assénat
Hello, We ran into an issue where the Linux omapdss driver would refuse to run because it couldn't find a VDDS_DSI regulator. Our design does not have such a regulator because it seems there is no such thing as an VDDS_DSI input pin. I made a patch to prevent searching and using a regulator on...
on
Jul 19, 2012
Forum Post:
MAX17041 LINUX DRIVER
RAJEEV BATTU
Dear ALL, I had interfaced MAX17041 fuel gauge IC to AM3517 for 2-cell battery monitoring. I had added slave address 0X36 " I2C_BOARD_INFO("max17040", 0x36)" in board file. And selected max17040 driver in menuconfig file. ALSO find the attachment..... Following is error...
on
Aug 18, 2012
1
2
3
4
5
»