Browse Topics
Amplifiers
Audio Amplifiers
High Speed Amplifiers
Precision Amplifiers
/etc... Amplifiers & Other Linear
Applications
Automotive
Medical & High Reliability
Motor Drivers
ARM® Processors
Sitara™ ARM®
Digital Signal Processors (DSP)
C5000 Ultra Low Power DSP
C6000 Multicore DSP
C6000 Single Core DSP
DaVinci™ Video Processors
OMAP™ Processors
Clocks & Timers
Data Converters
Audio Converters
High Speed Data Converters
Precision Data Converters
Video Converters
/etc... Data Converters
Development Tools
WEBENCH® Design Center
Code Composer Studio
TI C/C++ Compiler
DLP & MEMS
Embedded Software
Android
BIOS
Linux
Multimedia Software Codecs
StarterWare
WinCE
Interface
Consumer & Computing
Ethernet
Fiber Communication
High Speed Interface
Industrial Interface
/etc... Interface
Logic
Low Power RF & Wireless Connectivity
Microcontrollers
C2000™ Microcontrollers
Stellaris® ARM® Microcontrollers
MSP430™ Microcontrollers
Tiva™ ARM® Microcontrollers
Other Microcontrollers
Hercules™ Safety Microcontrollers
OMAP™ Applications Processors
Power Management
Battery Management
Digital Power
AC/DC and Isolated DC/DC Power
LED Drivers/LCD Bias
Linear Regulators
NexFET™ Power MOSFETs
Non-Isolated DC/DC
Power Modules
PMU
Power Interface
SIMPLE SWITCHER®
Sequencers
Supervisor and Reset IC
Wireless Power
/etc... Power
RF & Digital Radio
Digital Radio (GC Products)
High Performance RF Modulators, PLL and VCO products
/etc... RF
Other Analog & Touch
Imaging
Temperature Sensors
Touch
/etc... Analog
/etc Support
Custom Title
Support Forums
To post a question or find an answer, choose a topic from the "Browse Topics" navigation menu on the left.
Get this RSS feed
Tags
You have subscribed to this tag. To view or manage your tag subscriptions,
click here
.
Close
You have unsubscribed from this tag. To view or manage your tag subscriptions,
click here
.
Close
You are currently viewing:
BIOSPSP_ENG
6748
6748 -OMAP -L138
AUDIO
bios
bios 5
BIOS 6
bios/dsp
BIOS6
biospsp
C6000
C64x+
c6747
c6748
c674x
ccs v4
code Composer studio
dm6437
DM648
dsp bios
dsp/bios
DSP/BIOS 5
dsp/bios programming
EDMA
EDMA3
EDMA3 LLD
Related Posts
Forum Post:
Second EDMA_DRV_ChannelRequest fails on 6424
Jim Patterson16330
My second call to EDMA_DRV_ChannelRequest always fails with error code -139 (invalid parameters) My BIOS main function calls EDMA3_DRV_Create calls edma3OsSemCreate calls EDMA3_DRV_open Registers EDMA interrupts What I need to do is request EDMA channels in two tasks. One requests...
on
Mar 15, 2010
Forum Post:
FVID_queue/FVID_dequeue Issue
Franck
Hi, We are using a DM6437 to capture images with the VPFE Device Driver. We are manually controlling each image acquisition through a command sent to the image sensor, each one generating a single Frame Valid signal. We are working with three FVID_Frame buffers in the following way: 1- FVID_queue...
on
Mar 17, 2010
Forum Post:
Something about PSP Mcbsp Driver on DM6437
GU MO
Hi,everyone~ I am using the psp mcbsp driver for my mcbsp on dm6437. Here is some problem about the API. One of the prototypes of the API is : PSP_Result PSP_mcbspCreate (Uint32 instanceId, const PSP_mcbspDevParams *initCfg, Ptr Arg) the last parameter Ptr Arg is explained...
on
Mar 19, 2010
Forum Post:
BIOSUSB_01_00_00 has a bug?
Haoxing Li
Hi,gays I am using BIOSUSB package on OMAP-L137 for developing a USB communication system, and meet a trouble. I added a GPIO4-control task in BIOSUSB's usbhosthid example, but found that GPIO4-set register always be cleared ( set to 0 ) by BIOS/USB's Jungo_thread0. And if delect Jungo_thread0...
on
Mar 19, 2010
Forum Post:
I2C peripheral working in DMAInterrupt mode
hao zhang39149
Hi, I have been programming i2c peripheral in my own C6747 board using psp from TI. Up to now the i2c can work correctly by working in interrupt mode. But it can not output the right result while working in DMAInterrupt mode. By the way, the function, GIO_submit return the IOM_complete value, and the...
on
Mar 22, 2010
Forum Post:
BIOSPSP audio example for C674x
Yan8622
Hi, The audio example given in the C674x BIOSPSP package would stop running if the audio processing between SIO Rx and Tx takes too long. I think a better handling of this situation would be to skip the a few audio frames but without breaking anything. Any advice how to do that? Thanks
on
Mar 23, 2010
Forum Post:
OMAP-L137 Audio Codec register read via Aic31_AC_IOCTL_REG_READ not working.
Richard Bagdazian
I have written two routines for the purposes of accessing audio codec register settings on the OMAP-L137 EVM board. The code is shown below. The write routine seems to work fine ( I have implemented the fix to the audio driver that was referred to here) but the read routine always returns zeros no...
on
Mar 30, 2010
Forum Post:
reusing PSP audio example - does not link
Andreas Weishaupt
Hi all, I need to reuse the PSP McASP example in my own code. Since I've successfully compiled and run the example, I've simply copy-pasted most of the code from it into my own code, adapted McASP configuration for my own needs, adapted DSP/BIOS conf by looking at the DSP/BIOS conf of the...
on
Mar 31, 2010
Forum Post:
GPIO-BANK4&5 be always cleared by BIOSUSB's jungo_thread0
Haoxing Li
Hi, ============================ BIOSUSB version : 01_10_02 test board: OMAP-L137 evm ============================ The GPIO-BANK4_5's setdata register(addr: 0x01E26068) of OMAP-L137 is always cleared by jungo_thread0,and those pins goes low. So I can't keep them high statically. I have to...
on
Apr 1, 2010
Forum Post:
dynamically creating the biosusb tasks.
Peter Myerscough-Jackopson
I am having problems dynamically creating the tasks for the biosusb stack. I have created a program that can communicate over the usb using a custom CDC usb stack based upon the BIOSUSB driver, and if I placed the required jungo threads in the TCF file it all works.... BUT I cannot dynamically create...
on
Apr 1, 2010
Forum Post:
Re: the error of makehal_evmdm6437
David Friedland
I'll forward this on to the BIOS PSP team. I don’t know if they are maintaining these bat files and if they have made any changes to them. For many NSK drivers, they no longer support builds through batch files. The suggested way for building in changes to drivers into your application...
on
Apr 1, 2010
Forum Post:
DA830 DSK: Unable to open McASP driver to receive from AIC3106 DAC
David Kelly
CCS: Version: 4.1.1.00014 bios_6_21_00_13 pspdrivers_02_00_01 xdais_6_25_01_08 xdctools_3_16_02_32 edma3_lld_02_00_01_04 ipc_1_00_05_60 Platform: Spectrum Digital DA830 DSK Rev G Hello, I'm attempting to modify the working sample AIC3106 code that came from Spectrum Digital to use...
on
Apr 9, 2010
Forum Post:
C6455 with NDK 2.0.0: Jumbo size packets being broken up into several 1480 byte packets
g_dejesus
Hi, I'm running GigE connection speed between the C6455 DSP and a PC with a GigE 9k jumbo frame network card trying to stream real time video through the UDP port. On the PC side I setup the properties of the GigE card to have Jumbo Frames enabled. For some reason, the 7k image packets I'm...
on
Apr 9, 2010
Forum Post:
need Guidence to make intelligent switch with DM648
Ahmed 10245
hello all, I am working on DM648 with ndk1.92. I want to implement an intelligent switch application with the involvement of DSP processor of the topology mentioned below data from LAN ----->port0 (PHY 1) of dsp ------>port2( DSP processor) --------->port1(PHY 2) --------> to the PC ...
on
Apr 10, 2010
Forum Post:
Problems with sio_create function
Fernando Pimenta
Hi, I am using the mcbsp0 in slave mode, on the OMAP-L138 EVM Kit. I use the example that comes with the BIOSPSP_01_30_00 and all is working well if I use the hEdma[0]: Void mcbspDemoTask(Void) { // initialise the edma library if (IOM_COMPLETED != edma3init()) …………...
on
Apr 12, 2010
Forum Post:
How to access past frames on DM6437 by using FVID functions
Ahmet
Hi, I'm studying on video stabilization project on DM6437 . I could capture frames and display them out by using FVID_exchange function.And I could access pixels on current frame. I have to compare past frame and current frame .But I can only do operations on current frame. How can I...
on
Apr 14, 2010
Forum Post:
PSP lib builds for C6747
E2E_display_name_Mike
I am using version 01.30.00 PSP for the C6747 device. I notice the lib folders already contain pre-built libraries with the .a674 extension. I opened up the mcasp project in ccs4 and built the Debug and Release configurations but I do not get the same output. The only thing I changed was the extension...
on
Apr 22, 2010
Forum Post:
Re: read multiple images and store in different loacations
SATYA 48081
HI, I am using tms320dm6437EVM board .I am trying to grab three frames from camera in Y:Cb:Cr format and store just Y component of them in 2-dimensional variables. this is the code i use to capture thee different images and store this images in three different variables int I_frame[720][480],int...
on
Apr 27, 2010
Forum Post:
Problem with PSPIOM McBSP driver (Tx)
Pavel Livshits
Hello, I have board with DPS C6748 and 6 codecs so I'm using McBSP1 as TDM to send and receive the data. The drivers are provided by TI which are PSPIOM ver 01.30.01 and EDMA3 ver .01.11.00.03. The example in the PSPIOM using McBSP with SIO_issue and SIO_reclaim suits me well but for Rx only....
on
Apr 27, 2010
Forum Post:
Re: BIOS 6 and PSP v2 audio drivers!
David Friedland
The paste of the error looks unclear. Is the undefined symbol called "in"?
on
Apr 28, 2010
Forum Post:
Migrating DM642 PCI code to the DM647/8
Peter40529
Hi all, I'm working on migrating a DM642 system to a DM647 and am currently working on the PCI system. The DM642 code is based on the CSL libraries, and it looks like the DM647 will need to use the PSP PCI driver which seems to have a much different interface. My first fundamental question question...
on
May 1, 2010
Forum Post:
Configuring audio on DA830/OMAP L137 EVM!
Atmapuri
Hi! The audio sample application contains the code to record one channel (left from Line-in1) and playback one channel (left from line-out1 it seems). I am using PSP 02.00.01 for DA830. How can I configure the audio, to record both left and right channel and playback also both channels on line out...
on
May 1, 2010
Forum Post:
PSC Module!
Atmapuri
Hi! I found the following code in the EMV DA830 PSP 02.00.01 examples: var pscPrms = new Psc.Params(); pscPrms.devId = 1; Program.global.psc1 = Psc.create(pscPrms); What is the meaning of devId? Sometimes it is assigned a value of 1 and sometimes zero depending on the peripheral device. Is it...
on
May 3, 2010
Forum Post:
Two DM648 EMACs are not isolated perfectly?
Ho-Jin Lee
Hello. I have tried to use two DM648 EMACs separately. I have followed the instruction of http://tiexpressdsp.com/index.php/Using_two_DM648_EMACs_separately . My system network configuration is shown in the above picture. I want to isolate two EMACs. One EMAC is for data input. The other...
on
May 4, 2010
Forum Post:
Re: Why the dm648 network init stopped at SetPhyMode?
David Friedland
I'll ask the PSP team to respond...
on
May 5, 2010
1
2
3
4
5
»