Browse Topics
Amplifiers
Audio Amplifiers
High Speed Amplifiers
Precision Amplifiers
/etc... Amplifiers & Other Linear
Applications
Automotive
Medical & High Reliability
Motor Drivers
ARM® Processors
Sitara™ ARM®
Clocks & Timers
Data Converters
Audio Converters
High Speed Data Converters
Precision Data Converters
Video Converters
/etc... Data Converters
Development Tools
WEBENCH® Design Center
Code Composer Studio
TI C/C++ Compiler
Digital Signal Processors (DSP)
C5000 Ultra Low Power DSP
C6000 Multicore DSP
C6000 Single Core DSP
DaVinci™ Video Processors
OMAP™ Processors
DLP & MEMS
Embedded Software
Android
BIOS
Linux
Multimedia Software Codecs
StarterWare
WinCE
Interface
Consumer & Computing
Ethernet
Fiber Communication
High Speed Interface
Industrial Interface
/etc... Interface
Logic
Low Power RF & Wireless Connectivity
Microcontrollers
C2000™ Microcontrollers
Stellaris® ARM® Microcontrollers
MSP430™ Microcontrollers
Tiva™ ARM® Microcontrollers
Other Microcontrollers
Hercules™ Safety Microcontrollers
OMAP™ Applications Processors
Power Management
Battery Management
Digital Power
AC/DC and Isolated DC/DC Power
LED Drivers/LCD Bias
Linear Regulators
NexFET™ Power MOSFETs
Non-Isolated DC/DC
Power Modules
PMU
Power Interface
SIMPLE SWITCHER®
Sequencers
Supervisor and Reset IC
Wireless Power
/etc... Power
RF & Digital Radio
Digital Radio (GC Products)
High Performance RF Modulators, PLL and VCO products
/etc... RF
Other Analog & Touch
Imaging
Temperature Sensors
Touch
/etc... Analog
/etc Support
Custom Title
Support Forums
To post a question or find an answer, choose a topic from the "Browse Topics" navigation menu on the left.
Get this RSS feed
Tags
You have subscribed to this tag. To view or manage your tag subscriptions,
click here
.
Close
You have unsubscribed from this tag. To view or manage your tag subscriptions,
click here
.
Close
You are currently viewing:
CC2431
2.4 ghz
2.4ghz
802.15.4
adc
CC debugger
cc1100
cc1101
cc1110
cc1111
CC111x
cc2420
cc2430
cc2430db
cc2500
cc2510
cc2511
cc2520
cc2530
CC2530ZNP
cc2591
cc430
coordinator
FAQ
zigbee
Z-Stack
Related Posts
Forum Post:
Localization Engine + CC2591
Daimon2616
Hi everybody, Which are the consequences of adding a PA/LNA, like CC2591, to the CC2431 location engine? Will it work? I know that the gain is controllable, so at least we must take that into consideration in software. Other problems?
on
Aug 1, 2008
Forum Post:
Re: Localization Engine + CC2591
Hobbyist
Check out the these great papers on the CC2431 http://www.medialab.ch/archiv/pdf_studien_diplomarbeiten/da06/da2006-113_SensorNetworkSoccer.pdf http://bwrc.eecs.berkeley.edu/publications/2006/Publications/Theses/tufan_phd_thesis.pdf Maybe you can gain some info here, it is not directly an answer to your...
on
Aug 4, 2008
Forum Post:
Re: Location Engine CC2431
Hobbyist
Maybe use Kalman filter with CC2431. http://www.medialab.ch/archiv/pdf_studien_diplomarbeiten/da06/da2006-113_SensorNetworkSoccer.pdf http://bwrc.eecs.berkeley.edu/publications/2006/Publications/Theses/tufan_phd_thesis.pdf Hobbyist
on
Aug 4, 2008
Forum Post:
Re: Problems in Compiling CC2431 Location Engine Sample
LPRF Rocks the World
Hi, Interesting feedback :) With this on your displayed I am also sure the green LED is toggling too. Right? You will need to setup your IEEE address. Try to push the center of the joystick down and see what happens Hopefully this helps LPRF_Rocks
on
Aug 19, 2008
Forum Post:
Re: CC1110, Sleep, and Sleep Timer
RF4ALL
Hi, Try replace your xtal monitor instruction as follows: /*while(!(SLEEP & 0x40));*/ while(CLKCON & 0x40); This will monitor [CLKCON.OSC] to ensure that the [HS XOSC] is not only stable, but also actually applied as system clock source before continuing code execution. Cheers, RF4ALL
on
Aug 21, 2008
Forum Post:
Re: Programming custom CC2431 boards using the smartRF04eb
esy
Hi Alex, Yes, you can use the SmartRF04EB Evaluation Board as debugger for your CC2431 prototype, i.e. use as an in-circuit emulator with IAR EW8051 to debug your code. You will also be able to run our RF evaluation and radio configuration software called SmartRF Studio on your PC and use your prototype's...
on
Sep 15, 2008
Forum Post:
Re: CC2431
LPRF Rocks the World
rjacob, Check out this thread: https://community.ti.com/forums/p/189/430.aspx#430 A nice research paper on CC2431 usage: http://www.medialab.ch/archiv/pdf_studien_diplomarbeiten/da06/da2006-113_SensorNetworkSoccer.pdf LPRF Rocks the World
on
Sep 17, 2008
Forum Post:
Re: How to program a CC2431EM without a SmartRF04EB?
esy
Hi jorge, TI currently do not offer any alternative smaller/cheaper hardware for flash programming of CC243x devices other than the SmartRF04EB. However, there are some third party alternatives . (some of these are best suited for high-volume production). Here is a DIY alternative with open circuit...
on
Sep 25, 2008
Forum Post:
Re: Programming custom CC2431 boards using the smartRF04eb
esy
Hi ASHOK, ASHOK Hi, I am currently looking to purchase a smartRF04eb as part of a CC2431 Zigbee developmeny main interest is to be able to integrate the CC2431 into my own circuit designs, but I am wondering if the smartRF04eb facilitates the connection, maybe via a ribbon cable, to my custom boards...
on
Sep 28, 2008
Forum Post:
Re: A multinode locationing system with CC2431
LPRF Rocks the World
Hi Rex, How are things moving with your location project? Check out our Location Profile in the our Z-Stack for CC2430: swrc073d.zip (70MB) - contains ZStack-CC2430-1.4.3-1.2.1.exe (the "full" CC2430/31 Z-stack v.1.4.3 & Application Examples v.1.2.1) Note: See "Compatability...
on
Oct 2, 2008
Forum Post:
Z-tool setting in cc2430
baba sanfur
Hi All, I would like to use the Z-tool interface on the cc2430 (using z-stack), and I have three questions: 1. Is it possible to use the CTS / RTS signals while using the z-tool. What and where should I change the code? 2. How do I change the UART speed of the MCU to 115200 bps? 3. Can I set...
on
Oct 7, 2008
Forum Post:
Re: Code doesn't run on several chips
WorkingAgain?
Thank you guys for the reply. I will check out the frequency on these boards and will come back to you asap, but can take a while as there are more important things up this week, but you WILL hear from me. THX again. Hope it is that, so that I have 2-3 boards more for the network. FLO
on
Oct 20, 2008
Forum Post:
Re: endpoints joining mechanism
baba sanfur
Thanks for the quick answer! Let my refine my questions: If I set in hardware the first coordinator’s PAN ID to 0x0001, a second coordinator’s PAN id to 0x0002, and set PAN ID of all routers / endpoints to 0xFFFF – will the router be able to join both of them (once to the first coordinator...
on
Oct 22, 2008
Forum Post:
CC2431 Location Engine current consumption
RF-Explorer
Hi, Are there any published (or non-published!) figures for how much additional current is consumed by the Location Engine when enabled on the CC2431? Thanks.
on
Oct 24, 2008
Forum Post:
Re: CC2431 Location Engine current consumption
LPRF Rocks the World
RF Explorer, Current consumption yes, interesting topic. I like to use the comparsion done by a university in Switzerland: http://www.ceesar.ch/fileadmin/Dateien/PDF/designofaversatilelowcostIEEEmoduleforlongtermbatteryoperation_PaperEuZDC07_sk_final.pdf Check out the table on page 3 for the CC2430...
on
Oct 28, 2008
Forum Post:
Re: Programming custom CC2431 boards using the smartRF04eb
esy
Hi odel, the dongle in the eZ430 kits consists of two parts: the USB emulator board with USB connector (aka MSP-EZ430U), and a target board connected to it. The USB emulator can work as a debugger for the MSP430 on the target board. The debugger uses the 2-wire SPI-by-wire interface for the debugging...
on
Oct 30, 2008
Forum Post:
Re: CC2430 Startup
esy
Hi Ashok, Does the LCD of the SmartRF04EB Evaluation Board work in other situations? E.g. if you try to turn off the EB, remove the CC243xEM, and power the EB back on -- does the LCD say "Chipcon SRF04EB No EM detected!"? (just as a test that the LCD works). The CC2430 and the CC2431 are...
on
Oct 31, 2008
Forum Post:
How can i make this custom application?
jorge5224
Hi, i'm trying to make a custom application that sends messages from a pc by serial port to a coordinator and i have to send this message to an specific end point node, and then this node have to display this message througt its ports. and i also have to implement the location profile. i'm...
on
Oct 31, 2008
Forum Post:
Doubt with association list
lucholes
Hi, When a end device associate it with a router and then if it moves to another position it associate to another router. The first router that was father of this node, erase it from its association list?, to have an avaliable entry for other node. thanks!
on
Nov 12, 2008
Forum Post:
Re: Location Engine RefNode configuration
PME_BLUM
Wishmaster, If you study the location sample application code provided for the reference nodes you will see that the position is something that is stored in memory and can be updated in a variety of ways. The way we demonstrate in the sample code is for an incoming packet, initiated by the PC Tool...
on
Nov 13, 2008
Forum Post:
CC2431 and Wake-On-Radio
Mostafa Kassem
Greetings: According to the comparison matrix in the link listed below, the CC2431 can do WOR. However, I could not find any data to confirm this in the CC2420 transceiver or the CC2430 which the CC2431 is besed on. I would appreciate a pointer to where I can find information about the WOR on the...
on
Jan 7, 2009
Forum Post:
How to communicate two routers using Simple API?
Patrick9330
Does anyone know how to communicate two routers using Simple API? Can I bind a router with another router using Simple API in SimpleApp example? Should I bind the route or just let the it join in the existing network? How to do it by modifying SimpleController.c in SimpleApp ? Thanks.
on
Jan 9, 2009
Forum Post:
Re: CC2431 and Wake-On-Radio
Kjetil
Hi. The CC243/31 has a built in sleep timer that can be used for WOR-like functionality in systems where other MCUs are involved. Wake On Radio is usually a term used for tranceivers that can wake the MCU on packet reception only. Regards, Kjetil
on
Jan 9, 2009
Forum Post:
Problem when using osal_nv_write() in Z-Stack for CC2430
Patrick9330
Hi, I am now trying to write my own data into CC2430 flash. So I try to use osal_nv_write(uint16 id, uint16 ndx, uint16 len, void *buf ) to do that. #define ZCD_NV_DATAFRAME 0x0FF0 //user-defined ID static char _dataframe2[1]={'a'}; //my simple data to be stored in flash static char _dataOut...
on
Jan 22, 2009
Wiki Page:
MCU platforms supported by the TIMAC and ZigBee Z-StackTM software
Kjetil
Q: FAQ: MCU platforms supported by the TIMAC and ZigBee Z-StackTM software The recent releases of TIMAC (beginning with v1.0.1) supports TI MSP430, CC2430 and CC2431 (with 8051 MCU core) platforms. The recent releases of the Z-Stack (beginning with v1.4.0) supports Atmel AVR, CC2430 and CC2431 (with...
on
Nov 22, 2010
1
2
3
4
5
»