Browse Topics
Amplifiers
Audio Amplifiers
High Speed Amplifiers
Precision Amplifiers
/etc... Amplifiers & Other Linear
Applications
Automotive
Medical & High Reliability
Motor Drivers
ARM® Processors
Sitara™ ARM®
Digital Signal Processors (DSP)
C5000 Ultra Low Power DSP
C6000 Multicore DSP
C6000 Single Core DSP
DaVinci™ Video Processors
OMAP™ Processors
Clocks & Timers
Data Converters
Audio Converters
High Speed Data Converters
Precision Data Converters
Video Converters
/etc... Data Converters
Development Tools
WEBENCH® Design Center
Code Composer Studio
TI C/C++ Compiler
DLP & MEMS
Embedded Software
Android
BIOS
Linux
Multimedia Software Codecs
StarterWare
WinCE
Interface
Consumer & Computing
Ethernet
Fiber Communication
High Speed Interface
Industrial Interface
/etc... Interface
Logic
Low Power RF & Wireless Connectivity
Microcontrollers
C2000™ Microcontrollers
Stellaris® ARM® Microcontrollers
MSP430™ Microcontrollers
Tiva™ ARM® Microcontrollers
Other Microcontrollers
Hercules™ Safety Microcontrollers
OMAP™ Applications Processors
Power Management
Battery Management
Digital Power
AC/DC and Isolated DC/DC Power
LED Drivers/LCD Bias
Linear Regulators
NexFET™ Power MOSFETs
Non-Isolated DC/DC
Power Modules
PMU
Power Interface
SIMPLE SWITCHER®
Sequencers
Supervisor and Reset IC
Wireless Power
/etc... Power
RF & Digital Radio
Digital Radio (GC Products)
High Performance RF Modulators, PLL and VCO products
/etc... RF
Other Analog & Touch
Imaging
Temperature Sensors
Touch
/etc... Analog
/etc Support
Custom Title
Support Forums
To post a question or find an answer, choose a topic from the "Browse Topics" navigation menu on the left.
Get this RSS feed
Tags
You have subscribed to this tag. To view or manage your tag subscriptions,
click here
.
Close
You have unsubscribed from this tag. To view or manage your tag subscriptions,
click here
.
Close
You are currently viewing:
uart
2.4 GHz
2530
2540
2xx
3530
5505
5xx
6437
6678
6713
6713 DSK
6747
6748
674x
802.15.4
8148
814x
8168
adc
ADC10
ADC12
ais
aisgen
ALSA
am1808
Related Posts
Forum Post:
Re: S/W UART
BrandonElliott
Chakra, We actually have a code example that implements a software UART using the Timer_A. Please see the follwing zip file from www.MSP430.com for several different examples: http://www.ti.com/lit/zip/slac011 (namely, see msp430x11x1_ta_uart19200_01.c)
on
Aug 5, 2008
Forum Post:
Re: Serial Comm & TIMAC
LPRF Rocks the World
Hi, Have you check with a Serial Monitor Sniffer if anything from the Firmware is transmitted over the serial port to a PC? http://www.developer.com/net/cplus/article.php/633421 http://www.lvr.com/serport.htm http://www.serial-port-monitor.com/ LPRF_Rocks
on
Aug 19, 2008
Forum Post:
Re: Serial Comm & TIMAC
LPRF Rocks the World
Hi Ahmad, I would start just focus on getting the UART up and running, then your TMAC Sample App and next TIMAC + UART Check out the following Design Note just released: New design note: DN112 – Using UART in CC111xFx, CC2431x, and CC251xFx This design note explains the basic software use of the UART...
on
Sep 2, 2008
Forum Post:
help with SW Uart
nick836
Hello! I would to realize a SW uart that send my received packet to pc. I read software code on TI web site, but i don't want realize a echo program. I don't know how to implement this software... is there anyone who can help me, please? Thanks.
on
Oct 7, 2008
Forum Post:
Re: Problems on the DDK uart
TimHarron
Are you using the DM642 Video Port Mini-Driver in addition to the UART driver for the DM642 EVM? There was a problem in the VPMD which overwrites a few registers in the EVM's FPGA which essentially disables the UART. This is a simple fix, so if you are in fact using the VPMD and UART drivers I will...
on
Oct 13, 2008
Forum Post:
Re: Problems on the DDK uart
TimHarron
There are four hard register writes into FPGA registers that should be modified. I'll quote the code changes I made. Look for the comments with my initials. static void configSAA7105(SAA7105_Mode videoMode, Bool slaveModeEnable, SAA7105_AnalogFormat outMode, SAA7105_InputFormat inFormat, Bool enableBT656Sync...
on
Oct 15, 2008
Forum Post:
CC2430 UART transmit complete interrupt
colinb
Hi, I'm trying to use UART0 on a CC2430EM+SmartRF04EB to do RS-232 serial to my PC. I'm currently testing with the SDCC compiler. The problem is that the UTX0 interrupt is not getting called after sending a byte. The receive URX0 interrupt routine is working fine, and I'm doing exactly...
on
Oct 21, 2008
Forum Post:
CC2430EB - how to enable UART reception in SampleApp
akorhola
Hello, we have been using the Chipcon SmartRF04EB for a project, by implementing extra features into the provided SampleApp. Otherwise everything has been fine, but for some reason we can't get the UART RX interrupt to trigger at all. Transmitting from the board over UART works fine (Hyperterminal...
on
Nov 16, 2008
Forum Post:
Re: ADC help needed
BrandonElliott
Hi, The UART protocol is digital already, you should be able to plug and play with a code example for USCI channel A0 in UART mode (provided your device has the USCI). It should only be noted that the input voltage levels are valid per the spec in the datasheet.
on
Nov 18, 2008
Forum Post:
Serial port help needed
sam22
hey m using an Express card as my laptop does not has a serial port. When i use in device manager i see two COM port, one is of the express card & other is of MSP430, i select the one for express card & try to connect to hyperterminal. I am able to establish a connection but after that in the...
on
Nov 23, 2008
Forum Post:
Re: using UART0 and UART1 in DM6437
Bernie Thompson TI
The interrupt mode should work, the driver should be handling the HWI for you already based on how the example is setup. It may be worth trying out the example within C:\dvsdk_1_01_00_15\psp_1_00_02_00\pspdrivers\drivers\uart\sample to verify it works on your platform, the example utilizes the interrupt...
on
Nov 25, 2008
Forum Post:
Re: UART code needed
DerekC
sam22 I have another doubt is UCA0RXBUF on port 2 or port 4?? You were right to query about the port number. Got a reply from EPIC this morning and they pointed out that the Experimenter's Board (MSP430FG4618/F2013) uses P2.4 for UCA0TXD and P2.5 for UCA0RXD. I made the mods to msp430xG46x_uscia0_uart_9600...
on
Nov 26, 2008
Forum Post:
Re: UART code needed
DerekC
Sid, You should be able to use the PCMCIA card if it looks like a COM port to the laptop. Have a look in Control Panel->System->Hardware tab->Device Manager->Ports (COM & LPT), you should see one related to the PCMCIA card there. Then, use this port in the terminal application. ...
on
Nov 27, 2008
Forum Post:
CC2520DK kit and UART A1 problem
renka
Hi, I am currently working with CC2520DK kit.I have a stand-alone application,that activates UART A1 module of MSP4302618.The application writes data to PC and receives data from PC. The UART A0 of MSP430 works well,while UART A1 has only right TX functionality (Tx to PC,i am successufully write...
on
Dec 3, 2008
Forum Post:
Re: MSP430F2618 and NS LM9838 Bluetooth Chip
BrandonAzbell
dave I wanted to include a couple of examples from my code to make it easier to understand what I am doing. First, here is the section of code that sets the GPIO pin directions and functions: // Pin Pin # Direction Connections // P3.0 28 -> Flash CS // P3.1 29 <- Flash SDI // P3.2 30 ->...
on
Dec 6, 2008
Forum Post:
Re: MSP430F2618 and NS LM9838 Bluetooth Chip
dave6286
One additional data point. When I connect to the bluetooth chip on our board with my laptop, I do get 1 character from the BT chip [out of the 14 it sends when it gets a connection]. The other characters just never seem to make it to me. Would this indicate a baud rate problem or some other problem?
on
Dec 7, 2008
Forum Post:
Re: MSP430F2618 and NS LM9838 Bluetooth Chip
BrandonAzbell
Is the one character you do receive an expected value? If it is not the value you expect, I might expect a baud rate issue, but the only way to be sure is to use an oscilloscope to verify what is actually being sent and compare to what is being captured by the MSP430. What does your software do when...
on
Dec 7, 2008
Forum Post:
Re: 5xx LPM3 with UART wakeup?
BrandonAzbell
Have you looked at the code examples (SLAC166) provided on the MSP430F5438 Product Folder ? There are a couple of examples that configure the USCI for UART mode and use LPM0 and LPM3. They do use a different targeted baud rate, but this should provide some guidance. I realize this isn't a definitive...
on
Dec 7, 2008
Forum Post:
Re: CC2520DK kit and UART A1 problem
BrandonAzbell
What hardware are you using which has the MSP430F2618 on it? Would you be able to post your modifications to the MSP430x261x_uscia0_uart_01.c which have it configured to use UART A1?
on
Dec 7, 2008
Forum Post:
Re: MSP430F2618 and NS LM9838 Bluetooth Chip
BrandonAzbell
At this point, I think it is prudent to verify the baud rate before looking at other items. The USCI interface is going to be driven by the same clock for both the RX and TX operations. It would be easier to verify the baud rate by using some code to transmit a series of known values that you can then...
on
Dec 7, 2008
Forum Post:
Re: CC2480: Unclear about the documentation regarding the UART RTS and CTS pins
Dirty Harry
Hello - It looks like there are some typos on the CC2480 pin direction. Please remember that the CC2480 is a slave device in SPI mode and a DCE in UART mode (so a pin direction is opposite the intuitive direction implied by the name.) So, it is correct to realize that the CC2480 pin directions in UART...
on
Dec 10, 2008
Forum Post:
Re: CC2520DK kit and UART A1 problem
BrandonAzbell
You mentioned seeing signals on the RX line from the PC when using either USCI A0 or USCI A1. Where are you measuring these? Is it on the CCMSP-EM430F2618 board?
on
Dec 14, 2008
Forum Post:
Re: CC2480: Unclear about the documentation regarding the UART RTS and CTS pins
AnneauNîmes
Hello, I've a problem with the UART communication. We have set the following values durnig a RST low pulse (18ms) : CTS = 0 MRDY = 0 CFG1 = 0 CFG0 = 1 Unfortunately we have no response from the CC2480 after the RST pulse. Can someone tell me if this configuration is correct or why...
on
Dec 16, 2008
Forum Post:
Re: CC2520DK kit and UART A1 problem
BrandonAzbell
I would as a test to make sure there isn't any conflict that may be getting in your way.
on
Dec 18, 2008
Wiki Page:
How to setup a wireless UART with CC111x/CC251x devices
Kjetil
Q: FAQ: How to setup a wireless UART with CC111x/CC251x devices by 1184125 The CC111x/CC251x devices can easily be used to make a standard serial interface like UART wireless. Also covering CRC check and automatic retransmission for error free operation the wireless UART can run with an effective...
on
Nov 22, 2010
1
2
3
4
5
»