This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

Linux/TM4C123GE6PM: arch linux CCS install stuck at com.ti.debug

Prodigy 100 points

Replies: 23

Views: 7881

Part Number: TM4C123GE6PM

Tool/software: Linux

when I start to install CCS it works normall untill it went to install com.ti.debug.linux... and it stucks at this line.
I have opened task manager to watch the activity and it just runs some java the stuck.
debugserver_7.1.0.1971_install.logccs_7.1.0.00016.logccs_setup_7.1.0.00016_install.log

My version is the latest CCS7.1.0.00016_linux-x64

thanks in advance

  • Moving this to the Code Composer forum.

    Best Regards,
    Yordan

     


     Please make sure you read the forum guidelines first.

  • In reply to Yordan Kovachev:

    Hi Yordan,

    If possible, can you zip up the contents of install_logs/* and post them here? Also, please look for the bitrock*.log files in /tmp and zip up and post them. 

    Thanks

    Danish

  • In reply to danishinnis:

    I have already uploaded the three log files in my question. kindly check them.

    Thanks in advance.

  • In reply to islam omar:

    I'm sorry I only saw the one log file, my mistake.
    Did you kill off the debug server installer? I ask because something seems to have killed it off, from looking at the logs. Was anti-virus are you using?
    Danish
  • In reply to danishinnis:

    I have killed it as when the installer came to com.ti.debug.linux.... "in task manager it opens java and other programs" then the program freezes forever and do nothing in task manager, I even let them for a hole day to finish, but it just freezes at that line forever.

    I have no anti-virus installed

  • In reply to islam omar:

    Any suggestions?
  • In reply to islam omar:

    Hello,

    I am having the same issue when installing CCS7.1 as well as CCSv7.0 on Archlinux (64 Bit) and KDE (Plasma 5).

    It makes no difference whether installing as normal user or as root.

    When using "htop" is see 5 stucked process calls:

    /opt/ti/ccsv7/eclipse/downloads/ti_dspack_ibsetup_linux-x64_7.0.0.1808.run --mode unattended --ccs true --prefix /opt/ti/ccsv7 --eclipseprefix /opt/ti/ccsv7/eclipse

    In addition, I tried to run this stuck application manually, without the "--mode unattended" flag, while I left the previous setup is being stuck (otherwise it deletes this setup file). This opens another install wizard which successfully finishes installation of Debug Server. But on the final page (showing "Completing the Debug Server Setup Wizard"), if I press the "Finish" button, the wizard gets stuck (and the Finish button stays pressed). Furthermore, I get no output in console.

    Are there any suggestions on that?

    Regards,

    Robert

  • In reply to islam omar:

    On my system (Archlinux) I identified glibc-2.25 to be the cause of the problem. Downgrading to glibc-2.24 solved this issue.

    Tested with CCS7.1.0.00016_linux-x64.tar.gz

    Looks that something critical changed in glibc-2.25

    @TI: Please provide an updated package, which is also compatible with glibc-2.25.

    Regards,

    Robert
  • In reply to Robert Falkenberg:

    Now it stucks at InstallBins - CCS_INFO: Installing com.ti.cgt.tms470.16.linux-x64 (or at msp430 if I chose it).

    could you provide your system
  • In reply to Robert Falkenberg:

    It worked after downgrading all conflicting packges.
    thanks a bunch.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.