This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

CCS/MSP430F5438: Unfamiliar CCS error message

Part Number: MSP430F5438

Tool/software: Code Composer Studio

I get a similar message when Launching my application

An internal error occurred during: "Launching myapplication".  com/ti/dvt/energytrace/af/PowerActivity

And when I go to the preferences page

Windows -> Preferences > Code Composer Studio -> Advanced Tools -> EnergyTrace Technology

"Unable to create the selected preference page.   An error occurred while automatically activating bundle com.ti.dvt.energytrace (456)"

I've done two reinstalls of CCS to fight this issue.  

Any suggestions?

  • Guru 149215 points

    Please see item 7 in this page. Using a new workspace should resolve the error. 

    ____________________________________________________________________________

    Please click This Resolved My Issue if the reply answers your question.

    Search the wikis for common questions: Compiler, CCSv6, CCSv7
    Track a known bug with SDOWP. Enter the bug id in the "Find Record ID" box

  • In reply to AartiG:

    The specific problem had something to do with a corrupted workspace, or too little space left on the virtual drive the VMware instance of Windows had. I did some heavy trimming, both in my Host OS (my Mac OS laptop), then in that VMware instance of Windows. This included deleting most c:/TI directories (which could be reloaded), and reloading all the TI pieces. Including refreshing the CCS 7.4 (although not trying to move beyond that).

    Finally, when I reinstalled my workspace from backups, and GIT, it compiled cleanly. Whew! A couple of days lost on that. But I'm happy I'm back developing.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.