This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

CCS/CC1310: Stack usage missing when --printf_support nofloat

Part Number: CC1310

Tool/software: Code Composer Studio

With '--printf_support full' View->Stack usage displays values for  __TI_printfi (called from vsnprintf).

Switching to '--printf_support nofloat` removes stack usage information from __TI_printfi.

With huge stack usage in __TI_printfi, it is a bit annoying

Is there some way to fix this? I can annotate __TI_printfi, estimating from full version, but it is a bit tedious.

Regards,

Petr

  • Guru 153005 points
    Petr,

    Can you share a simple project that demonstrates this issue so we can reproduce the behavior and submit a report to track and address this?

    ____________________________________________________________________________

    Please click This Resolved My Issue if the reply answers your question.

    Search the wikis for common questions: Compiler, CCSv6, CCSv7
    Track a known bug with SDOWP. Enter the bug id in the "Find Record ID" box

  • In reply to AartiG:

    Hello,

    any project using sprintf should do, in examples only rfEasyLinkNp is actually using it (other examples do avoid it at cost of readability)

    1. import rfEasyLinkNp_CC1310_LAUNCHXL_tirtos_ccs (\ti\simplelink_cc13x0_sdk_2_10_00_36\examples\rtos\CC1310_LAUNCHXL\easylink\rfEasyLinkNp\tirtos\ccs\rfEasyLinkNp_CC1310_LAUNCHXL_tirtos_ccs.projectspec)

    2. build project and display Stack Usage. Descending almost any function with high stack usage will lead to __TI_printfi (atCtrlRxMsg - processRx - AtTerm_sendStringUi8Value - sprintf - __TI_printfi - 640 stack bytes)

    3. Change project properties: CCS build - ARM compiler - Advanced Options - Language Options - Level of printf support to anything but full

    4. Rebuild, reload stack usage - __TI_printfi stack information is missing

  • In reply to AartiG:

    AartiG
    Can you share a simple project that demonstrates this issue so we can reproduce the behavior and submit a report to track and address this?

    The attached simple project for a TM4C129 device which calls sprintf() demonstrates this with CCS 8.1.0.00011 and TI ARM compiler v18.1.3.

    1) With the --printf_support set to "full" the CCS Stack Usage view shows usage for the __TI_printfi function:

    And with --printf_support set to "full" the linker map shows there is a symbol called "__TI_printfi".

    2) Whereas when --printf_support is set to "nofloat" the CCS Stack Usage view reports that the stack info for __TI_printfi is missing:

    And with --printf_support set to "full" the linker map shows there is a symbol called "__TI_printfi_nofloat". I.e. with the suffix "_nofloat".

    I think this might be the same issue as reported in CCS/MSP430FG4618: CCS 7.2 Stack Usage can under-report the stack size requirement when Function Symbol Aliasing occurs. While CODEGEN-3595 which was raised for the referenced thread is reported as fixed in ARM_18.1.2.LTS, there is the following in the Release Notes for CODEGEN-3595:

    Currently, the Stack Assistant GUI is not capable of showing both the aliased and alias function names for calls to aliased functions-- this will require a future update.

    2502.TM4C_sprintf_stack_usage.zip

  • Guru 153005 points

    In reply to Petr Ledvina:

    With the rfEasyLinkNp_CC1310_LAUNCHXL_tirtos_ccs project compiled with --printf_support=nofloat, I see the following (__TI_printfi_nofloat and __TI_scanfi_nofloat)
    in the Stack Usage view. As Chester pointed out the function names are different when code is built with nofloat option.

    Do you not see these in your Stack Usage view?

    ____________________________________________________________________________

    Please click This Resolved My Issue if the reply answers your question.

    Search the wikis for common questions: Compiler, CCSv6, CCSv7
    Track a known bug with SDOWP. Enter the bug id in the "Find Record ID" box

  • In reply to AartiG:

    AartiG
    With the rfEasyLinkNp_CC1310_LAUNCHXL_tirtos_ccs project compiled with --printf_support=nofloat, I see the following (__TI_printfi_nofloat and __TI_scanfi_nofloat)
    in the Stack Usage view. As Chester pointed out the function names are different when code is built with nofloat option.

    The issue in the CCS Stack Usage view is that __TI_printfi_nofloat is shown as an orphan function which doesn't appear to be called in the program, and as a result the reported stack usage for sprintf, and therefore any callers of sprintf, is lower that the actual stack usage.

    In the attached example which uses --printf_support=nofloat a post-build rule was added to run the cg_xml call_graph utility. The output of call_graph (Debug/TM4C_sprintf_stack_usage_call_graph.txt) in the attached project shows the same issue as the CCS Stack Usage view is that __TI_printfi_nofloat is shown as an orphan function whose stack usage does not contribute to the stack usage of sprintf:

    __TI_printfi_nofloat : wcs = 632
    |  __aeabi_errno_addr : wcs = 0
    |  _ltostr : wcs = 32
    |  |  ULL$DIV : wcs = ???
    |  |  strlen : wcs = 0
    |  atoi : wcs = 16
    |  memccpy : wcs = 8
    |  memset : wcs = 20
    |  strlen : wcs = 0
    |  wcslen : wcs = 0
    
    __aeabi_uldivmod : wcs = 20
    
    _c_int00_noargs : wcs = 136
    |  __TI_auto_init : wcs = ???
    |  __mpu_init : wcs = ???
    |  _system_pre_init : wcs = 0
    |  exit : wcs = ???
    |  main : wcs = 128
    |  |  sprintf : wcs = 40
    |  |  |  __TI_printfi : wcs = ???

    Looking at how sprintf is implemented in the TI ARM v18.1.3.LTS shows:

    a) The lib/src/sprintf.c source file contains the implementation of sprintf which simply calls __TI_printfi to perform the work. The implementation of sprintf is the same regardless of the --printf_support option.

    b) The lib/src directory contains three .c source files used to compile different implementations of printf support:

    _printfi.c implements the __TI_printfi function for use by --printf_support=full

    _printfi_min.c implements the __TI_printfi_minimal function for use by --printf_support=minimal

    _printfi_nf.c implements the __TI_printfi_nofloat function for use by --printf_support=nofloat

    I think the linker uses the --printf_support to modify a call to __TI_printfi to either a call to __TI_printfi / __TI_printfi_minimal / __TI_printfi_nofloat function depending upon the use of either --printf_support=full / --printf_support=minimal / --printf_support=nofloat.

    If armdis is used to disassemble the out file created with --printf_support=nofloat then sprintf is shown as calling __TI_printfi_nofloat which is OK:

    ~/ti/ccs810/ccsv8/tools/compiler/ti-cgt-arm_18.1.3.LTS/bin/armdis TM4C_sprintf_stack_usage.out 
    Disassembly of TM4C_sprintf_stack_usage.out:
    <snip>
    000d30:              sprintf:
    000d30:               .thumb
    000d30:              .text:sprintf:
    000d30: 0FB4             PUSH            {R0, R1, R2, R3}
    000d32: 80B5             PUSH            {R7, LR}
    000d34: 02AF             ADD             R7, SP, #8 
    000d36: ADF1100D         SUB.W           R13, R13, #16
    000d3a: 0290             STR             R0, [SP, #8]
    000d3c: 7A68             LDR             R2, [R7, #4]
    000d3e: 0192             STR             R2, [SP, #4]
    000d40: 094B             LDR             R3, $C$CON1 [0xd68]
    000d42: 0093             STR             R3, [SP]
    000d44: 094B             LDR             R3, $C$CON2 [0xd6c]
    000d46: 391D             ADDS            R1, R7, #4
    000d48: 21F00301         BIC.W           R1, R1, #3
    000d4c: 091D             ADDS            R1, R1, #4
    000d4e: 01A8             ADD             R0, SP, #4 
    000d50: 02AA             ADD             R2, SP, #8 
    000d52: FFF759FA         BL              __TI_printfi_nofloat [0x208]
    000d56: 0299             LDR             R1, [SP, #8]
    000d58: 0022             MOVS            R2, #0
    000d5a: 0A70             STRB            R2, [R1]
    000d5c: 04B0             ADD             SP, #16
    000d5e: BDE88040         LDMIA.W         R13!, {R7, R14}
    000d62: 04B0             ADD             SP, #16
    000d64: 7047             BX              R14
    000d66: C046             MOV             R8, R8
    000d68:              $d:
    000d68:              $C$CON1:
    000d68: F30D            .half		 0x0DF3
    000d6a: 0000            .half		 0x0000
    000d6c:              $C$CON2:
    000d6c: 4B0E            .half		 0x0E4B
    000d6e: 0000            .half		 0x0000

    However the output from armofd -cg, which is extracted from the debug information and forms the input to the CCS Stack Usage view, shows sprintf is shown as calling __TI_printfi, rather than the actual __TI_printfi_nofloat which is linked to the program:

    ~/ti/ccs810/ccsv8/tools/compiler/ti-cgt-arm_18.1.3.LTS/bin/armofd -cg TM4C_sprintf_stack_usage.out 
    <?xml version="1.0" encoding="ISO-8859-1" ?>
    <ofd>
       <banner>TI ARM Object File Display Unix v18.1.3.LTS</banner>
       <copyright>Copyright (c) 1996-2017 Texas Instruments Incorporated</copyright>
       <name>TM4C_sprintf_stack_usage.out</name>
       <call_graph>
          <function>
             <name>sprintf</name>
             <stack_size>0x28</stack_size>
             <makes_indirect_call>false</makes_indirect_call>
             <file>sprintf.c</file>
             <line>0x40</line>
             <address>0xd30</address>
             <is_combined>false</is_combined>
             <definition_seen>true</definition_seen>
             <has_stack_usage_info>true</has_stack_usage_info>
             <producer>TI TI ARM C/C++ Codegen Unix v18.1.3.LTS Copyright (c) 1996-2017 Texas Instruments Incorporated</producer>
             <callee>__TI_printfi</callee>
          </function>

    I think the TI linker needs to be changed so that when --printf_support changes the actual implementation of the __TI_printfi function in the RTS which gets linked, that the debug information is updated accordingly so programs which process the call graph to determine the worst case stack usage can follow the actual called functions.

    6708.6443.TM4C_sprintf_stack_usage.zip

  • In reply to Chester Gillon:

    Thanks to Chester Gillon for a test case.  I used it to analyze the situation.  I agree with his analysis ...

    Chester Gillon
    I think the TI linker needs to be changed so that when --printf_support changes the actual implementation of the __TI_printfi function in the RTS which gets linked, that the debug information is updated accordingly so programs which process the call graph to determine the worst case stack usage can follow the actual called functions.

    I filed CODEGEN-5179 in the SDOWP system to have this investigated.  You are welcome to follow it with the SDOWP link below in my signature.

    Thanks and regards,

    -George


    TI C/C++ Compiler Forum Moderator
    Please click This Resolved My Issue on the best reply to your question
    The CCS Youtube Channel
     has short how-to videos
    The 
    Compiler Wiki answers most common questions
    Track an issue with SDOWP. Enter your bug id in the Search box.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.