Hi All,
I have a code which compiles without any errors. However, when the CCS tries to build the ARM linker I get an error which I just can't seem to be able to figure:
'Building target: CC9000_B.out'
'Invoking: ARM Linker'
"C:/ti/ccsv5/tools/compiler/arm_5.0.4/bin/armcl" -mv7M4 --abi=eabi -me -g --diag_warning=225 --display_error_number --diag_wrap=off --stack_overflow_check -z --stack_size=2000 -m"CC9000_B.map" -i"C:/ti/ccsv5/tools/compiler/arm_5.0.4/lib" --reread_libs --warn_sections --display_error_number --diag_wrap=off --xml_link_info="CC9000_B_linkInfo.xml" --rom_model -o "CC9000_B.out" "./main.obj" "./System.obj" "./File_IO.obj" "./Control_Functions.obj" "./Common.obj" -l"C:\ti\TivaWare_C_Series-1.0\driverlib\ccs\Debug\driverlib.lib" -l"libc.a"
<Linking>
undefined first referenced
symbol in file
--------- ----------------
handle_stkovf C:\ti\ccsv5\tools\compiler\arm_5.0.4\lib\rtsv7M4_T_le_v4SPD16_eabi.lib<stkchk_t2.obj>
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "CC9000_B.out" not built
>> Compilation failure
gmake: *** [CC9000_B.out] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****
Thanks in advance for the help.