Tool/software: Code Composer Studio
Good day!
I try to compile simple program: sum numbers at array only if current number (at array) >0.
But i can not complile code:
.ref _c_int00 ; _c_int00: .data array1: .int 2,-1,47,-99 size .set 4 .text MVKL .S1 array1,A3 MVKH .S1 array1,A3 MVK .S1 size,A2 MVK .S1 0,A0 MVK .S2 0,B2 MVK .S1 0,A6 MVK .S1 0,A4 MVK .S1 0,A5 LOOP: SUB .L1 A2,1,A2 ;A2 := A2 - 1 ; MVK .S2 -1,B3 LDW .D1 *A3[A2],B2 NOP 4 CMPGT .L1 A5,0,A6 NOP 6 [A6]ADD .L1 A5,A0,A4 NOP 5 [A2]B .S1 LOOP NOP 5 ERROR! at line 24: [E0003] Illegal register for conditional [A6]ADD .L1 A5,A0,A4
I try many ways to fix this problem, but i can not do this.
If i change A6 to B2 (for example), it compiles well.
What i do wrong?
Thank you!
Target is: TMS320C6ZXX.
Code Composer 3.3.