This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: C5505 Programming PCB standalone

Tool/software: Code Composer Studio

Hi, 

I'm try to make my project persistent on a self-made SoC based on C5505 PCB.

I Use programmer.out that I used with c5505 eZdsp demo board (programmer.out)

When I specify the executable (.bin) absolute path, the download seem to start but never ends.

Input your binary file path...
C:\Users\marti\Desktop\BACKUP\DC2017\project\BootImageTool\DC2017.bin
SPI EEPROM...
Writing data to device...
Opening C:\Users\marti\Desktop\BACKUP\DC2017\project\BootImageTool\DC2017.bin...
Input file opened

I'm using XDS100 V3 debug probe.

Any tip? It's quite urgent, please.

Thanks in advance

Paolo