Tool/software: Code Composer Studio
Hello,
I have encountered a troubling issue in which when i try to debug a function the debugger is totally out of sync - behaves as if the shown source is not the one that generated to code.
All optimizations are OFF everything is up to date.
some other functions on the same file seemed to be OK.
I have tried splitting the file into two files and then it seems to be working as it should.
Is there a limit as to the length of a source file? if so what is it and is there a way to change/control it? (i am not sure that this is actually the issue - all i know that this enabled me to debug the function i could not before)
are the any another ideas as to why this may happen and how to resolve it -- i rather, if possible, have one single file for these functions.
Thanks
Guy