Tool/software: Code Composer Studio
I'm having trouble with CCS's (version 8.2.0) syntax highlighting feature: when adding a class to a C/C++ project, classes do not behave as expected: autocompletion of class members and method doesn't work, the class' name is not highlighed as a type, and F3 cannot find the declaration. If I substitute class by struct in the class declaration, F3 works but nothing else.
It seems that my header files are being indexed as C files and not as C++ files, since everything C works. However, when importing an example project, classes are indexed as expected. Is there something I forgot to configure? Where do I set up whether the indexer will read header files as C or C++?