Other Parts Discussed in Thread: CC2650
Tool/software: Code Composer Studio
HI TI and forum users
I am trying to use the SAP example provided in the SDK BLE plugin V 1.40.00.42
I am not sure if this is the proper forum section to place my question in, but here goes:
I can't get the FreeRTOS example to work. I get no errors and no warning but when the code is on the board northing happens.
In debug mode i get stuck at configASSERT( pcName ); in task.c line 864, and acoording to RTOS weppage
pcName: A descriptive name for the task. This is mainly used to facilitate debugging, but can also be used to obtain a task handle.
The maximum length of a task's name is set using the configMAX_TASK_NAME_LEN parameter in FreeRTOSConfig.h.
i am not sure why it would be stopping there, but i am quite new to the RTOS side of embedded programming.
Also i have changed northing in the original code.
So i was wondering if anybody else have the same problem.
and sorry for any grammatik errors, if not understood i will try explain it better
Thank you for your time
Mikkel
Some info on my setup.
CC2650 BP running on the MSP432P401R
Using the simplelink sdk ble plugin v1.40.00.42
and the CCS version is 8.1.0.00011
My FreeRTOS version is 10.1.1
i am also using the BLE scanner app on my android phone to pick op the BLE signal.
TI-RTOS
and FreeRTOS i have cleared the terminal for not getting confused