Other Parts Discussed in Thread: SIMPLELINK-CC2640R2-SDK, CC2640R2F, SYSBIOS, CC2650, CC2640
Tool/software: Code Composer Studio
Hi,
I did the following test and find out that using CCS ubuntu version cause no UART log problem.
The same steps work fine on Windows and macOS.
My steps:
1. Install CCS on Ubuntu 18.04/Windows
2. From CCS "Getting Started" page to download example for and import project
3. Build one of the example application code
4. Run->Load->Select program to load-> tof_initiator
5. using minicom to open ttyACM0 port
6. Press the reset button on CC2640R2 board
7. The console window should output something. (It works fine on Windows, but nothing on Ubuntu)
Environment:
OS: Ubuntu 18.04
CCS version: Version: 8.2.0.00007
TI platform: CC2640R2
SimpleLink CC2640R2 Software Development Kit: SIMPLELINK-CC2640R2-SDK_2.30.00.28
Example code:
../blestack/tof_initiator
../blestack/tof_responder
../blestack/aoa_sender
../blestack/aoa_receiver
Please help on this and tell me what logs or information you need so that I can get for you.
Thanks,
Stanley