Other Parts Discussed in Thread: UCD3138A64, UCD3138, UNIFLASH
Tool/software: Code Composer Studio
We are using UCD3138A64 along with the XDS100V2 debug probe.
As suggested in the earlier thread,
When we load the .x0 file while the box is checked, we get the following output
When we load the .out file , we get the following output.
The console displays "Device ID Validation option not selected."
The above two outputs are not similar to the one's shown in the TI UCD3138 training video series.
Also, the USB to GPIO probe is not used instead we have powered the board externally and we are using XDS100V2 JTAG to program the board.
So is that JTAG sufficient for all the necessary operations we will be performing?