Original question:
CCS: Code Composer Studio™ forum
Replies: 10
Views: 234
Part Number: TMS320F2808
Tool/software: Code Composer Studio
I am getting started to program a processor board with TMS320F2808.
I am using Code Composer Studio 8 and and emulator XDS200. The communication of the hardware with CCS seems to work.
I want to begin with examples downloaded from http://www.ti.com/tool/SPRC191
I want to proceed exactly according to the related document "DSP280x_HeaderFiles_QuickStart_Readme.pdf"
I am at the page 6 of the document and I am trying to execute the step A. I want to execute Load GEL command from File menu.
The command does not exist in the File menu. I execute the steps B and C opening the file. I want to continue executing the step D.
I cannot find the pull down menu containing the command Load_and_Build_Project.
Because the Code Composer Studio does not behave as described I am completely impotent to get started.
Please tell me what is wrong in the document "DSP280x_HeaderFiles_QuickStart_Readme.pdf" or what mistake I have done
and tell me how can I click step by step to run an example from the collection, for example GPIO program with GPIO pins oscillating?
My email address is following <pstros@hotmail.com>
The document you are referring to was written for CCSv3.x. The CCS version you are using (v8) is considerably different compared to 3.x. CCS3.x is not supported any more. The F2808, being a relatively old device in our portfolio, is not supported on C2000ware. You have two options:
1. Move to a newer device, so that you get the benefit of seamless support in C2000ware. Meaning, you can come up to speed quickly with the examples provided in C2000ware.
2. You can still run the examples provided in the DSP Header files. However, you cannot use the procedure outlined in the Readme doc. You must use the Project-->Import Legacy CCS3.3 project option. This allows you to import .PJT files from CCS3.x projects.
Hareesh
If the issue is resolved, please close the forum post.
In reply to Hareesh J:
In reply to Ken Schachter:
Dear Friend, Mr. Hareesh,
you recommended me to use in CCS 8 the command Project => Import Legcy CCSv3.3 Projects.
After I imported the file .pjt" and clicked Next => Finish,
I obtained following error message
Issues that may require your attention were encountered while migrating the
project(s). Please see the 'project.log' file, in the root of each project, for details.
The log file contains (Censored! Please refrain from using expletive words) that cannot help me:
!CONFIGURATION: 'com.ti.ccstudio.buildDefinitions.C2000.Release.1114035985' [Thu Jan 24 17:47:11 CET 2019]
!TOOL: 'com.ti.ccstudio.buildDefinitions.C2000_18.1.exe.compilerRelease.1623379253'
!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C2000_18.1.exe.compilerRelease.1623379253::!--symdebug:dwarf
In reply to Peter Visnyi:
Peter,
I don’t know which GPIO pins you tried to toggle, but could it be that the GPIO pins you tried to toggle are multiplexed with the SPI function? (Please look at Table 4-16 of SPRS230N for muxing options).
Did you try Example_280xGpioToggle.c in C:\tidcs\c28\DSP280x\v160\DSP280x_examples\gpio_toggle directory? This is a tested code and should work "as is". Else you can use the attached code, which is just a few lines.
What hardware are you using? Is it your own board?
Teamviewer is blocked by our network; I cannot use it.
#include "DSP280x_Device.h" main() { asm(" EALLOW"); /* Disable Watchdog */ SysCtrlRegs.WDCR = 0x006F; /* Configure GPIO pin */ GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 0; GpioCtrlRegs.GPADIR.bit.GPIO0 = 1; /* Toggle GPIO pin */ while(1) { GpioDataRegs.GPATOGGLE.bit.GPIO0 = 1; } }
I tried to run the code send by you. There are two problems.
1. When building the project, the compiler cannot find the header files. I have installed header files from the SPRC191 file downloaded from internet. The installer created the header files structure exactly according to the official document "DSP280x_HeaderFiles_QuickStart_Readme.pdf", they are in "C:\tidcs" directory. However, the Code Compose Studio cannot find the header files. I have copied the "DSP280x_Device.h" into the project directory in my work space. The compiler could not find additional header files included in "DSP280x_Device.h". If I copy all required header files into my project directory, still the compiler cannot build the project because the important structures are defined as external:
extern volatile struct SYS_CTRL_REGS SysCtrlRegs; extern volatile struct GPIO_CTRL_REGS GpioCtrlRegs; extern volatile struct GPIO_DATA_REGS GpioDataRegs;
I can correct the mistake deleting the word "extern" and the project can be built. Because of many problems I made my own single header file "GPIO_Example.h" extracting only useful definitions from all header files. You can see it below at the end. I solved the problem by non standard method. Please tell me what mistake I have done that the Code Composer Studio cannot find the header files and the compiler tells that the structures are not defined and I had to correct mistakes in header files.
2. The second problem is the real problem that I cannot solve. I had to make changes in the code sent by you, I replaced the "DSP280x_Device.h" by my own header file "GPIO_Example.h". I can build the project, to load it into RAM memory and to run it. I discovered that after I run the program, the processor jumps into SPI boot mode. This behavior does not depend at all on the program code in the "main.c" file. By oscilloscope I can see at the four pins of SPIA interface typical behavior
of clock, data and control signals exactly corresponding to SPI boot mode.
I have a professional processor board from a frequency converter for induction motors
having a connector for an emulator.I have a complete scheme of the board forbidden to publish, and it is evident that all boot modepins have pull up resistors resulting in 111 boot mode (Boot to Flash).I cannot understand the reason why the processor jumps into SPI boot moderegardless of what program I write.
I think that you cannot find answer to this problem.I am asking you to send me answer at least to my header files problem No 1.
This is my own header file code
typedef unsigned int Uint16;typedef unsigned long Uint32;
struct GPACTRL_BITS { // bits description Uint16 QUALPRD0:8; // 7:0 Qual period Uint16 QUALPRD1:8; // 15:8 Qual period Uint16 QUALPRD2:8; // 23:16 Qual period Uint16 QUALPRD3:8; // 31:24 Qual period};
union GPACTRL_REG { Uint32 all; struct GPACTRL_BITS bit;};
struct GPBCTRL_BITS { // bits description Uint16 QUALPRD0:8; // 7:0 Qual period Uint16 rsvd1:8; // 15:8 reserved Uint16 rsvd2:16; // 31:16 reserved};
union GPBCTRL_REG { Uint32 all; struct GPBCTRL_BITS bit;};
struct GPA1_BITS { // bits description Uint16 GPIO0:2; // 1:0 GPIO0 Uint16 GPIO1:2; // 3:2 GPIO1 Uint16 GPIO2:2; // 5:4 GPIO2 Uint16 GPIO3:2; // 7:6 GPIO3 Uint16 GPIO4:2; // 9:8 GPIO4 Uint16 GPIO5:2; // 11:10 GPIO5 Uint16 GPIO6:2; // 13:12 GPIO6 Uint16 GPIO7:2; // 15:14 GPIO7 Uint16 GPIO8:2; // 17:16 GPIO8 Uint16 GPIO9:2; // 19:18 GPIO9 Uint16 GPIO10:2; // 21:20 GPIO10 Uint16 GPIO11:2; // 23:22 GPIO11 Uint16 GPIO12:2; // 25:24 GPIO12 Uint16 GPIO13:2; // 27:26 GPIO13 Uint16 GPIO14:2; // 29:28 GPIO14 Uint16 GPIO15:2; // 31:30 GPIO15};
struct GPA2_BITS { // bits description Uint16 GPIO16:2; // 1:0 GPIO16 Uint16 GPIO17:2; // 3:2 GPIO17 Uint16 GPIO18:2; // 5:4 GPIO18 Uint16 GPIO19:2; // 7:6 GPIO19 Uint16 GPIO20:2; // 9:8 GPIO20 Uint16 GPIO21:2; // 11:10 GPIO21 Uint16 GPIO22:2; // 13:12 GPIO22 Uint16 GPIO23:2; // 15:14 GPIO23 Uint16 GPIO24:2; // 17:16 GPIO24 Uint16 GPIO25:2; // 19:18 GPIO25 Uint16 GPIO26:2; // 21:20 GPIO26 Uint16 GPIO27:2; // 23:22 GPIO27 Uint16 GPIO28:2; // 25:24 GPIO28 Uint16 GPIO29:2; // 27:26 GPIO29 Uint16 GPIO30:2; // 29:28 GPIO30 Uint16 GPIO31:2; // 31:30 GPIO31};
struct GPB1_BITS { // bits description Uint16 GPIO32:2; // 1:0 GPIO32 Uint16 GPIO33:2; // 3:2 GPIO33 Uint16 GPIO34:2; // 5:4 GPIO34 Uint16 rsvd1:2; // 7:6 reserved Uint16 rsvd2:8; // 15:8 reserved Uint16 rsvd3:16; // 31:16 reserved};
struct GPB2_BITS { // bits description Uint16 rsvd1:16; // 15:0 reserved Uint16 rsvd2:16; // 31:16 reserved};
union GPA1_REG { Uint32 all; struct GPA1_BITS bit;};
union GPA2_REG { Uint32 all; struct GPA2_BITS bit;};
union GPB1_REG { Uint32 all; struct GPB1_BITS bit;};
union GPB2_REG { Uint32 all; struct GPB2_BITS bit;};
struct GPADAT_BITS { // bits description Uint16 GPIO0:1; // 0 GPIO0 Uint16 GPIO1:1; // 1 GPIO1 Uint16 GPIO2:1; // 2 GPIO2 Uint16 GPIO3:1; // 3 GPIO3 Uint16 GPIO4:1; // 4 GPIO4 Uint16 GPIO5:1; // 5 GPIO5 Uint16 GPIO6:1; // 6 GPIO6 Uint16 GPIO7:1; // 7 GPIO7 Uint16 GPIO8:1; // 8 GPIO8 Uint16 GPIO9:1; // 9 GPIO9 Uint16 GPIO10:1; // 10 GPIO10 Uint16 GPIO11:1; // 11 GPIO11 Uint16 GPIO12:1; // 12 GPIO12 Uint16 GPIO13:1; // 13 GPIO13 Uint16 GPIO14:1; // 14 GPIO14 Uint16 GPIO15:1; // 15 GPIO15 Uint16 GPIO16:1; // 16 GPIO16 Uint16 GPIO17:1; // 17 GPIO17 Uint16 GPIO18:1; // 18 GPIO18 Uint16 GPIO19:1; // 19 GPIO19 Uint16 GPIO20:1; // 20 GPIO20 Uint16 GPIO21:1; // 21 GPIO21 Uint16 GPIO22:1; // 22 GPIO22 Uint16 GPIO23:1; // 23 GPIO23 Uint16 GPIO24:1; // 24 GPIO24 Uint16 GPIO25:1; // 25 GPIO25 Uint16 GPIO26:1; // 26 GPIO26 Uint16 GPIO27:1; // 27 GPIO27 Uint16 GPIO28:1; // 28 GPIO28 Uint16 GPIO29:1; // 29 GPIO29 Uint16 GPIO30:1; // 30 GPIO30 Uint16 GPIO31:1; // 31 GPIO31};
struct GPBDAT_BITS { // bits description Uint16 GPIO32:1; // 0 GPIO32 Uint16 GPIO33:1; // 1 GPIO33 Uint16 GPIO34:1; // 2 GPIO34 Uint16 rsvd1:13; // 15:3 reserved Uint16 rsvd2:16; // 31:16 reserved};
union GPADAT_REG { Uint32 all; struct GPADAT_BITS bit;};
union GPBDAT_REG { Uint32 all; struct GPBDAT_BITS bit;};
struct GPBPUD_BITS { // bits description Uint16 GPIO32:1; // 0 GPIO32 Uint16 GPIO33:1; // 1 GPIO33 Uint16 GPIO34:1; // 2 GPIO34 Uint16 GPIO35:1; // 3 GPIO35 Uint16 rsvd1:12; // 15:4 reserved Uint16 rsvd2:16; // 31:16 reserved};
union GPBPUD_REG { Uint32 all; struct GPBPUD_BITS bit;};
struct GPIOXINT_BITS { // bits description Uint16 GPIOSEL:5; // 4:0 Select GPIO interrupt input source Uint16 rsvd1:11; // 15:5 reserved};
union GPIOXINT_REG { Uint16 all; struct GPIOXINT_BITS bit;};
struct GPIO_CTRL_REGS { union GPACTRL_REG GPACTRL; // GPIO A Control Register (GPIO0 to 31) union GPA1_REG GPAQSEL1; // GPIO A Qualifier Select 1 Register (GPIO0 to 15) union GPA2_REG GPAQSEL2; // GPIO A Qualifier Select 2 Register (GPIO16 to 31) union GPA1_REG GPAMUX1; // GPIO A Mux 1 Register (GPIO0 to 15) union GPA2_REG GPAMUX2; // GPIO A Mux 2 Register (GPIO16 to 31) union GPADAT_REG GPADIR; // GPIO A Direction Register (GPIO0 to 31) union GPADAT_REG GPAPUD; // GPIO A Pull Up Disable Register (GPIO0 to 31) Uint32 rsvd1; union GPBCTRL_REG GPBCTRL; // GPIO B Control Register (GPIO32 to 63) union GPB1_REG GPBQSEL1; // GPIO B Qualifier Select 1 Register (GPIO32 to 47) union GPB2_REG GPBQSEL2; // GPIO B Qualifier Select 2 Register (GPIO48 to 63) union GPB1_REG GPBMUX1; // GPIO B Mux 1 Register (GPIO32 to 47) union GPB2_REG GPBMUX2; // GPIO B Mux 2 Register (GPIO48 to 63) union GPBDAT_REG GPBDIR; // GPIO B Direction Register (GPIO32 to 63) union GPBPUD_REG GPBPUD; // GPIO B Pull Up Disable Register (GPIO32 to 63) Uint16 rsvd2[33];};
struct GPIO_DATA_REGS { union GPADAT_REG GPADAT; // GPIO Data Register (GPIO0 to 31) union GPADAT_REG GPASET; // GPIO Data Set Register (GPIO0 to 31) union GPADAT_REG GPACLEAR; // GPIO Data Clear Register (GPIO0 to 31) union GPADAT_REG GPATOGGLE; // GPIO Data Toggle Register (GPIO0 to 31) union GPBPUD_REG GPBDAT; // GPIO Data Register (GPIO32 to 63) union GPBDAT_REG GPBSET; // GPIO Data Set Register (GPIO32 to 63) union GPBDAT_REG GPBCLEAR; // GPIO Data Clear Register (GPIO32 to 63) union GPBDAT_REG GPBTOGGLE; // GPIO Data Toggle Register (GPIO32 to 63) Uint16 rsvd1[16];};
struct GPIO_INT_REGS { union GPIOXINT_REG GPIOXINT1SEL; // XINT1 GPIO Input Selection union GPIOXINT_REG GPIOXINT2SEL; // XINT2 GPIO Input Selection union GPIOXINT_REG GPIOXNMISEL; // XNMI_XINT13 GPIO Input Selection Uint16 rsvd2[5]; union GPADAT_REG GPIOLPMSEL; // Low power modes GP I/O input select};
struct XCLK_BITS { // bits description Uint16 XCLKOUTDIV:2; // 1:0 XCLKOUT Divide Ratio Uint16 XCLKOUTDAT:1; // 2 reserved for TI use only Uint16 X1DAT:1; // 3 reserved for TI use only Uint16 XCLKINDAT:1; // 4 reserved for TI use only Uint16 rsvd1:3; // 7:5 reserved Uint16 X1CNT:4; // 11:8 reserved for TI use only Uint16 XCLKINCNT:4; // 15:12 reserved for TI use only};
union XCLK_REG { Uint16 all; struct XCLK_BITS bit;};
struct PLLSTS_BITS { // bits description Uint16 PLLLOCKS:1; // 0 PLL lock status Uint16 CLKINDIV:1; // 1 CLKIN div by 2 Uint16 PLLOFF:1; // 2 PLL off bit Uint16 MCLKSTS:1; // 3 Missing clock status bit Uint16 MCLKCLR:1; // 4 Missing clock clear bit Uint16 OSCOFF:1; // 5 Oscillator clock off Uint16 MCLKOFF:1; // 6 Missing clock detect Uint16 rsvd2:9; // 15:7 reserved};
union PLLSTS_REG { Uint16 all; struct PLLSTS_BITS bit;};
struct HISPCP_BITS { // bits description Uint16 HSPCLK:3; // 2:0 Rate relative to SYSCLKOUT Uint16 rsvd1:13; // 15:3 reserved};
union HISPCP_REG { Uint16 all; struct HISPCP_BITS bit;};
struct LOSPCP_BITS { // bits description Uint16 LSPCLK:3; // 2:0 Rate relative to SYSCLKOUT Uint16 rsvd1:13; // 15:3 reserved};
union LOSPCP_REG { Uint16 all; struct LOSPCP_BITS bit;};
struct PCLKCR0_BITS { // bits description Uint16 rsvd1:2; // 1:0 reserved Uint16 TBCLKSYNC:1; // 2 EWPM Module TBCLK enable/sync Uint16 ADCENCLK:1; // 3 Enable high speed clk to ADC Uint16 I2CAENCLK:1; // 4 Enable SYSCLKOUT to I2C-A Uint16 rsvd2:1; // 5 reserved Uint16 SPICENCLK:1; // 6 Enable low speed clk to SPI-C Uint16 SPIDENCLK:1; // 7 Enable low speed clk to SPI-D Uint16 SPIAENCLK:1; // 8 Enable low speed clk to SPI-A Uint16 SPIBENCLK:1; // 9 Enable low speed clk to SPI-B Uint16 SCIAENCLK:1; // 10 Enable low speed clk to SCI-A Uint16 SCIBENCLK:1; // 11 Enable low speed clk to SCI-B Uint16 rsvd3:2; // 13:12 reserved Uint16 ECANAENCLK:1; // 14 Enable system clk to eCAN-A Uint16 ECANBENCLK:1; // 15 Enable system clk to eCAN-B};
union PCLKCR0_REG { Uint16 all; struct PCLKCR0_BITS bit;};
struct PCLKCR1_BITS { // bits description Uint16 EPWM1ENCLK:1; // 0 Enable SYSCLKOUT to EPWM1 Uint16 EPWM2ENCLK:1; // 1 Enable SYSCLKOUT to EPWM2 Uint16 EPWM3ENCLK:1; // 2 Enable SYSCLKOUT to EPWM3 Uint16 EPWM4ENCLK:1; // 3 Enable SYSCLKOUT to EPWM4 Uint16 EPWM5ENCLK:1; // 4 Enable SYSCLKOUT to EPWM5 Uint16 EPWM6ENCLK:1; // 5 Enable SYSCLKOUT to EPWM6 Uint16 rsvd1:2; // 7:6 reserved Uint16 ECAP1ENCLK:1; // 8 Enable SYSCLKOUT to ECAP1 Uint16 ECAP2ENCLK:1; // 9 Enable SYSCLKOUT to ECAP2 Uint16 ECAP3ENCLK:1; // 10 Enable SYSCLKOUT to ECAP3 Uint16 ECAP4ENCLK:1; // 11 Enable SYSCLKOUT to ECAP4 Uint16 rsvd2:2; // 13:12 reserved Uint16 EQEP1ENCLK:1; // 11 Enable SYSCLKOUT to EQEP1 Uint16 EQEP2ENCLK:1; // 11 Enable SYSCLKOUT to EQEP2};
union PCLKCR1_REG { Uint16 all; struct PCLKCR1_BITS bit;};
struct PLLCR_BITS { // bits description Uint16 DIV:4; // 3:0 Set clock ratio for the PLL Uint16 rsvd1:12; // 15:4 reserved};
union PLLCR_REG { Uint16 all; struct PLLCR_BITS bit;};
struct LPMCR0_BITS { // bits description Uint16 LPM:2; // 1:0 Set the low power mode Uint16 QUALSTDBY:6; // 7:2 Qualification Uint16 rsvd1:7; // 14:8 reserved Uint16 WDINTE:1; // 15 Enables WD to wake the device from STANDBY};
union LPMCR0_REG { Uint16 all; struct LPMCR0_BITS bit;};
struct SYS_CTRL_REGS { union XCLK_REG XCLK; // 0 union PLLSTS_REG PLLSTS; // 1 Uint16 rsvd1[8]; // 2-9 union HISPCP_REG HISPCP; // 10: High-speed peripheral clock pre-scaler union LOSPCP_REG LOSPCP; // 11: Low-speed peripheral clock pre-scaler union PCLKCR0_REG PCLKCR0; // 12: Peripheral clock control register union PCLKCR1_REG PCLKCR1; // 13: Peripheral clock control register union LPMCR0_REG LPMCR0; // 14: Low-power mode control register 0 Uint16 rsvd2; // 15: reserved Uint16 rsvd3; // 16: reserved union PLLCR_REG PLLCR; // 17: PLL control register Uint16 SCSR; // 18: System control and status register Uint16 WDCNTR; // 19: WD counter register Uint16 rsvd4; // 20 Uint16 WDKEY; // 21: WD reset key register Uint16 rsvd5[3]; // 22-24 Uint16 WDCR; // 25: WD timer control register Uint16 rsvd6[6]; // 26-31};
volatile struct GPIO_CTRL_REGS GpioCtrlRegs;volatile struct GPIO_DATA_REGS GpioDataRegs;volatile struct SYS_CTRL_REGS SysCtrlRegs;
#define DINT asm(" setc INTM")#define EALLOW asm(" EALLOW")#define EDIS asm(" EDIS")
cregister volatile unsigned int IFR;cregister volatile unsigned int IER;