Tool/software: Code Composer Studio
Hi,
I started building the application over the simple_peripheral_observer example from the ble_examples-simplelink_cc2640r2_sdk-2.20 I found online. Then later I deleted this sdk and the CCS by takes up a compatible version of the sdk i.e. 2.30.0.28.
I checked the Project->Properties->CCS Build->ARM Compiler->Include Options and nothing seems to be pointing to the sdk 2.20 path which of course doesn't exist. Below is the warnings I get.
Invalid project path: Include path not found (/home/vinaydivakar/Desktop/ble_examples-simplelink_cc2640r2_sdk-2.20/examples/rtos/CC2640R2_LAUNCHXL/bleapps/simple_peripheral_observer/src/stack). Product 'SimpleLink CC2640R2 SDK' v2.20.0.49 is not currently installed. A compatible version 2.30.0.28 will be used.
I also searched in the .cproject file and there is no path defined in there. In the .ccsproject file, I changed the "SDK: 2.20.0.49" to "SDK:2.30.00.28" as shown below.
<templateProperties value="id=simple_peripheral_observer_cc2640r2lp_stack_library.projectspec.simple_peripheral_observer_cc2640r2lp_stack_library,products=com.ti.SIMPLELINK_CC2640R2_SDK:2.30.00.28;com.ti.rtsc.XDCtools:3.50.02.20,target=ti.targets.arm.elf.M3,platform=ti.platforms.simplelink:CC2640R2F,buildProfile=release,isHybrid=true,configuroOptions=--compileOptions ${COMPILER_FLAGS}"/> <origin value="/home/vinaydivakar/Desktop/Adroit/Projects_Gitkraken/ruru_cc2640r2/ruru_cc2640r2/CCS_ibeaconTxRx/simple_peripheral_observer_cc2640r2lp_stack_library"/>
And I also checked the paths in Project Properties->Linked Resources and the ${COM_TI_SIMPLELINK_CC2640R2_SDK_INSTALL_DIR} is resolved to the sdk 2.30.00.28.So no issues here as well.
Could someone advise on how to get rid of the above warnings?