Part Number: BEAGLEBK
Tool/software: Code Composer Studio
As per am335x processor sdk am335x starting guide , i followed the steps .
I able to see uboot.img and mlo in BOOT partition and rootfs file system rootfs partition .
boot up the beagle bone with sd card and able to login root partition .
uname -r shows--- 4.14.79-gbde58ab01e of beagle bone sd card image .
CCS version : 9.0.0
As per starting guide i created a remote setup for hello world example code . when i tried to connect to remote ccs prompt says :
Failed to connect SFTP subsystem: Remote host may not have sftp-server installed : java.io.IOException: inputstream is closed.
checked beagle bone ip address .