Other Parts Discussed in Thread: UNIFLASH,
Tool/software: Code Composer Studio
1. The LauchXL boards (two of them) worked fine out of the box: I was able to test the Bluetooth Project Zero by connecting to the board form my Androind phone, as described in the page (Out of the Box Experiemce):
http://dev.ti.com/tirex/explore/node?node=ADuSIrFg2kUHlTd9Kp0MqQ__pTTHBmu__LATEST
2. Then I wanted to try out the Zigbee Project Zero described in the page. I used Unifash to clear existing firmware on two boards and loaded the coordinator and end device firmware.
http://dev.ti.com/tirex/explore/node?node=AIHpFUnGAZPCyIyMVNwlJA__pTTHBmu__LATEST
3. However, I ran into trouble connecting to either board using putty. So I tried to restore the firmware to factory setting (using the right button and the reset button). I also tried to flash the hex file of the ble5stack projectzero from
C:\ti\simplelink_cc13x2_26x2_sdk_3_10_00_53\source\ti\ble5stack\hexfiles\cc13x2r1\ble5_project_zero_cc13x2p2lp_app_FlashROM_Release_unsecure.hex.
4. But the Android app does not seem to recognize the launchpads as BLE devices. My suspicion is that the firmware erase step in the Zigbee Project Zero 9( Step 0) instructions may have erased ket firmware sectors that should not have been erased.
How do I set the boards to their factory setting so that the Bluetooth Out of the Box ProjectZero works?
Thanks,
Siva