Tool/software: Code Composer Studio
I have a IWR1443BOOST. Information of Pc display is ok On high accuracy Visualizer. But I use oscilloscope, I can`t see signal on IR_RS232_Tx.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
I have a IWR1443BOOST. Information of Pc display is ok On high accuracy Visualizer. But I use oscilloscope, I can`t see signal on IR_RS232_Tx.
Hi Guo,
How are you probing the RS232_Tx pin? According to the schematic, R169 is not installed so you won't see anything on the BP/LP Connector.
Simply install the R169 and you can probe pin 5 on the J6 connector to see the signal.
Cheers,
Akash
Pin 5 on the J6 connector is RS232_Tx pin,Pin 7 on the J6 connector is RS232_Rx pin。But I can probe pin 5 and pin 7 on the J6 connector to see the signal.Pin 7 on the J6 connector should not see signal. Why is this?
Hi Guo,
The Resistors R169 and R166 which enable you to probe AR_RS232TX and AR_RS232RX are not installed by default, you must install these resistors in order to probe these pins on the connector.
Cheers,
Akash