This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] CCS: CCSv9 - Installer in text mode (no gui, only cli-usage)

Intellectual 450 points

Replies: 3

Views: 1095

Tool/software: Code Composer Studio

Hi,

i'm planning on using the ccs-projects on a build server (debian) for automated builds. Therefore i need ccs available in command-line-mode.

What i'm trying right now is installing CCSv9 with the installer using the following call:

./ccs_setup_linux64_9.1.0.00010.bin --mode text

This call doesn't work. The error message says:

Error copying file from /tmp/bitrock_installer_32242.log to /home/<username>/Downloads/CCS9.1.0.00010_linux-x64/***unknown variable installer_location***/ccs_9.1.0.00010.log
:Destination not writable

My assumption is that there's some missing variable in the installer regarding the variable 'installer_location' which leads to this error.

How can i fix that?

By the way: Is it even possible to configure and build CSS projects on a no-gui/cli-only server (debian)? On my local machine with CCS installed via the GUI-Installer i can call and trigger builds using the eclipsec --noSplash .... ... commands. 

Thanks for your help.

Best regards,

Jan

  • Guru 315615 points

    Hi Jan,

    '--mode text' is not supported. For a GUI-less install use:

    ./ccs_setup_linux64_9.1.0.00010.bin --mode unattended --prefix <install location>

    This will do a full install to the specified location

    Jan Feld
    By the way: Is it even possible to configure and build CSS projects on a no-gui/cli-only server (debian)? On my local machine with CCS installed via the GUI-Installer i can call and trigger builds using the eclipsec --noSplash .... ... commands. 

    yes the same commands can be used to build CCS projects from CLI. It is actually 'eclipse' on Linux:

    http://software-dl.ti.com/ccs/esd/documents/ccs_projects-command-line.html#working-with-ccs-linux

    Thanks

    ki

    -----------------------------------

    Did you read the CCS Forum Guidelines & FAQ? If not, PLEASE read it. If you haven't read it in awhile, please read it again to see if any updates were made.

    Having CCS problems? Check out the CCS Troubleshooting Guide

    Looking for CCS Training/Documentation? Check out the CCS Resources page

    Curious about the status of a bug and know the tracking ID? Track it via the public bug tracking portal

    NOTE: When a bug is filed and a tracking ID is provided, the thread may then be suggested as "TI Thinks Resolved". Why? Please read the first FAQ of the CCS Forum Guidelines & FAQ

  • In reply to Ki:

    Thanks for the answer!

    Best regards,

    Jan

  • Guru 315615 points

    NOTE: As of Code Composer Studio version 9.2.0, the installer command line parameters have changed. Please read the below link for more details on using CCS 9.2.0+ installer via CLI:

    https://software-dl.ti.com/ccs/esd/documents/ccs_installer-cli.html

    Thanks

    ki

    -----------------------------------

    Did you read the CCS Forum Guidelines & FAQ? If not, PLEASE read it. If you haven't read it in awhile, please read it again to see if any updates were made.

    Having CCS problems? Check out the CCS Troubleshooting Guide

    Looking for CCS Training/Documentation? Check out the CCS Resources page

    Curious about the status of a bug and know the tracking ID? Track it via the public bug tracking portal

    NOTE: When a bug is filed and a tracking ID is provided, the thread may then be suggested as "TI Thinks Resolved". Why? Please read the first FAQ of the CCS Forum Guidelines & FAQ

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.