Tool/software: TI C/C++ Compiler
Win7 32bit, CCS 6.2, F28023.
I am including rts2800_ml.lib in my code, and it seems very large.
Upon looking at the map, I see functions like fputs.obj, fprintf.obj, strcpy.obj, and many more.
I am not using these functions in my code.
As I understand it, by default, the compiler shouldn't be including these functions if they are uncalled.
Is there a trick to getting CCS to not include those functions during compile, or do I have to make a custom library with only the functions I need?
As an aside, Is there a way I can get CCS to show me a map of all functions and functions they call, including the RTS?
For example, if main() calls myfunc() and myfunc calls atoi() and atoi() calles someother(), is there a way I can get CCS to show me that in some form of graphical manner?
Thanks Mark.