Other Parts Discussed in Thread: UNIFLASH, CC3220SF, SEGGER
Tool/software: Code Composer Studio
Hi,
I made a custom board with CC3220MODASF. I have 4 JTAG signals accessible (TDO, TDI, TCK and TMS). I have configured the SOP pins to 000 i.e 4W JTAG
I connect XDS110 probe with our board using the 20 to 10 pin adapter.
The SOP jumpers are set to pull-down (FUNCTIONAL_4WJ) and the board is externally powered (3 V).
I have read earlier e2e community forum on the same issues of " could not connect to the target " and you are suggesting to use Uniflash software & UART to change the module to development mode from production mode.
But the problem is that we dont have the UART pins available in our custom board. But we have given test points for the SPI serial flash.
Can we use these SPI serial flash pins to change the mode of the module to development mode using uniflash or some other software ?
Can we use Over the Air programming to solve these issue ??
Or can you suggest any other way to change the module to development mode other than UART boot loading method
Appreciate your help at the earliest ....!!
Regards,
Rajesh