Tool/software: Code Composer Studio
Hi
I am on linux 18.04, CCS 9, and I imported the uartecho_CC2650STK_TI project in the IDE (on the PC):
I can build the project, but when I launch a debug session, I get :
Cortex_M3_0: GEL Output: Memory Map Initialization Complete.
Cortex_M3_0: Failed to retrieve the Wait in Reset Mode: (Error -6311) PRSC module failed to write to a register. (Emulation package 8.2.0.00004)
Cortex_M3_0: Error connecting to the target: (Error -6311) PRSC module failed to write to a register. (Emulation package 8.2.0.00004)
here is the screenshot. When I click on TestConnection, I get a success:
.....
The JTAG DR Integrity scan-test has succeeded.
[End: Texas Instruments XDS110 USB Debug Probe]
I am not sure if I have hooked up the board the right way, here is a photo ( with the XDS110):
Thanks
Peter