Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Hello,
I have a problem using functions in epwm.h (part of c2000ware driverlib).
I am not able to change any register value using epwm module functions. The epwm inline function executes, but register value remains unchanged.
The GPIO form the same driverlib works fine, and I am able to run and compile the code fine.
EPWMLOCK register is 0x00000000.
My pwm setup code is below.
Best regards,
Tom.
void INIT_epwm(void) { //! ePWM3 SETUP uint16_t periodCount = 4095U; //! Reset the ePWM3 counter EPWM_setTimeBaseCounter(EPWM3_BASE, 0U); //! Set the prescaler EPWM_setClockPrescaler(EPWM3_BASE, EPWM_CLOCK_DIVIDER_1, EPWM_HSCLOCK_DIVIDER_1); //! Set the time base period (reset value) EPWM_setTimeBasePeriod(EPWM3_BASE, periodCount); //! Set period load mode to load from shadow register EPWM_setPeriodLoadMode(EPWM3_BASE, EPWM_PERIOD_SHADOW_LOAD); //! Set time base counter mode to up-down EPWM_setTimeBaseCounterMode(EPWM3_BASE, EPWM_COUNTER_MODE_UP_DOWN); //! Set the period load event (from shadow register) EPWM_selectPeriodLoadEvent(EPWM3_BASE, EPWM_SHADOW_LOAD_MODE_COUNTER_ZERO); //! Set on which event will compare registers load from their respective... //! ...shadow load registers. Will be set for CMPA and CMPB. EPWM_setCounterCompareShadowLoadMode(EPWM3_BASE, EPWM_COUNTER_COMPARE_A, EPWM_COMP_LOAD_ON_SYNC_CNTR_ZERO); EPWM_setCounterCompareShadowLoadMode(EPWM3_BASE, EPWM_COUNTER_COMPARE_B, EPWM_COMP_LOAD_ON_SYNC_CNTR_ZERO); //! Set initial duty cycle to 50% EPWM_setCounterCompareValue(EPWM3_BASE, EPWM_COUNTER_COMPARE_A, (uint16_t) 0.5*periodCount); EPWM_setCounterCompareValue(EPWM3_BASE, EPWM_COUNTER_COMPARE_B, (uint16_t) 0.5*periodCount); //! Set action qualifier to load on counter zero EPWM_setActionQualifierShadowLoadMode(EPWM3_BASE, EPWM_ACTION_QUALIFIER_A, EPWM_AQ_LOAD_ON_CNTR_ZERO); //! In future, set action qualifier T1 to trigger on overcurrent //! Also set the appropriate action qualifier action make outputs HI-Z //! Add dead-band functions in future //! Add trip-zone functions in future //! Set EPWM interrupt source as time-base counter = ZERO EPWM_setInterruptSource(EPWM3_BASE, EPWM_INT_TBCTR_ZERO); //! Set EPWM interrupt event count to one event EPWM_setInterruptEventCount(EPWM3_BASE, 1); //! Add ADC trigger source in future }