This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TLV320ADC3101: TMS320DM368 can't identify TLV320ADC3101

Part Number: TLV320ADC3101

Tool/software: Code Composer Studio

when i am using DM368 to co-work with TLV320ADC3101, it can't identify the soundcard successfully

the register returned as below

​         PCR   = 0

​        MCR  =0 

​         SRGR =0x20000001

And the code log show as bleow

[    1.290000] asoc: tlv320aic3x <-> davinci-i2s mapping ok

​[    1.320000] ALSA device list:

​[    1.320000]   #0: DaVinci EVM (tlv320aic3x)

 

 Does it mean the soundcard already recognized by the CPU?

 However, when i type in arecord -I

it shows: no soundcards found...

so why did it happen, did it mean the registers had not been configured in the rightway?