Tool/software: Code Composer Studio
Having trouble changing the sampling rate for the ADC. The fastest input signal ADC can sample right now is only 1 or 2 Hz, which is not useful at all. And once the input signal has a frequency higher than 5Hz, the data that ADC samples just do not seem correct. Also, in Sensor Controller Studio, how do I make the minimum task iteration smaller than 10ms?
The code I use is an example code that is called rfWsnNode_CC2640R2_LAUNCHXL_tirtos_ccs. I attached part of the code that is from NodeTask.c at the bottom. I did not change anything and it is straight from the example code. This code also will read the output from Sensor Controller Studio, which I also attached below.