Tool/software: Code Composer Studio
Dear TI experts,
for I couple of CCS versions I had the impression, that some values in the debug perspective's expressions view were wrong. Now I updated to version 10.0.0.00010, but the problem is still the same. The displayed value is wrong and it changes from time to time (becomes yellow highlighted). Thus I had a look on the variables in the memory browser. In the memory browser the bytes do not change (as I expect) and they represent exactly the value I expect:
The variables making trouble are most often dFactor and beActive, but also pFactor and iFactor less frequent.
As you can see in the memory browser the bytes corresponding to dFactor are not aligned and represent a value of 5.25128235e-05 (according to matlab). They do NOT change over time.
For array index 0 dFactor is at 0x2000C3D8 (aligned) and correcty displayed as 5.25128235e-05.
Could you solve this annoying bug?
If you need any more information please let me know.