Tool/software: Code Composer Studio
I want to output to a serial program such as hyperterm and not the console. So I follow the Wiki link at https://processors.wiki.ti.com/index.php/Printf_support_for_MSP430_CCSTUDIO_compiler
I then use the following: int16_t fputc(int16_t my_char, register FILE *_fp) as shown in the Wiki. Not to drop back a moment, this all works fine when using IAR and the function int16_t putchar(int16_t c)
The problem is when output data goes to the serial program (putty), it is missing all the %d, %x, %f, etc. and I do have the Level of printf/scanf set to FULL in Language Options.
Outputs
Version: ..
should output
Version: 3.0.7
Notice its missing the 3, 0. 7 in this case the %d.
All the output displays fine on the Console.
Has anyone seen this problem?
Thanks,
-Jim