WEBENCH® Tools/OMAP-L138: OMAP-L138: ROTS/OMAP-L138/lcdk-06.00.00.07-Windows-x86-Install:CCS-Error

Prodigy 240 points

Replies: 4

Views: 103

Part Number: OMAP-L138

Tool/software: WEBENCH® Design Tools

Hi

Error happens. A message dialog is copied to TI_07.
I reeasrch some of WEB site, and arranged a file(c:\ti\ccs910\ccs\eclipse\eclipse.ini), Is is proper?

Please.
Tell me.

fuasa

4 Replies

  • Hi,

    Could you explain your use case in more details? What are you doing exactly? What is the error that happens?

    Best Regards,
    Yordan

     


     Please make sure you read the forum guidelines first.

  • In reply to Yordan Kovachev:

    Hi

    Yordan

    Thank you for reading.

    This is an error.

    I referenced the following web-site, and arranged characters are shown in RED.

    log

    '-startup
    plugins/org.eclipse.equinox.launcher_1.5.0.v20180512-1130.jar
    --launcher.library
    plugins/org.eclipse.equinox.launcher.win32.win32.x86_64_1.1.700.v20180518-1200
    --launcher.defaultAction
    openFile
    --launcher.XXMaxPermSize
    512M
    --launcher.appendVmargs
    -vmargs
    -Dosgi.requiredJavaVersion=1.8
    -Dosgi.dataAreaRequiresExplicitInit=true
    -Xms40m
    -Xmx512m
    --add-modules=ALL-SYSTEM

    Thank you very much.

    fuasa

  • In reply to userasagonta55:

    T_7.xlsx
    error Diglog

    fuasa

  • Guru 298875 points

    In reply to userasagonta55:

    Hello,

    Note that CCS typically uses the settings in ccstudio.ini instead of eclipse.ini. If you wish to change the heap size, make it to ccstudio.ini.

    Also, what version of CCS are you using?

    Thanks

    ki

    -----------------------------------

    Did you read the CCS Forum Guidelines & FAQ? If not, PLEASE read it. If you haven't read it in awhile, please read it again to see if any updates were made.

    Having CCS problems? Check out the CCS Troubleshooting Guide

    Looking for CCS Training/Documentation? Check out the CCS Resources page

    Curious about the status of a bug and know the tracking ID? Track it via the public bug tracking portal

    NOTE: When a bug is filed and a tracking ID is provided, the thread may then be suggested as "TI Thinks Resolved". Why? Please read the first FAQ of the CCS Forum Guidelines & FAQ