• TI Thinks Resolved

WEBENCH® Tools/MSP-EXP430FR5969: Interface Board Flashing issue

Prodigy 40 points

Replies: 6

Views: 68

Part Number: MSP-EXP430FR5969

Tool/software: WEBENCH® Design Tools

Hi am Using Texas Instruments SmartRF Flash Programmer, connected it to IC M430FR5729 via JTag communication cable and the IC Is connected to 12V DC Supply, when I start to do flashing, the SmartRF Flash Programmer is showing that the device is unknown, But no other Application is actively using the MSP-FET, (Please take a look at the Attached Screen shot ) When i click on perform actions button the window is closing automatically

enter image description here