• TI Thinks Resolved

WEBENCH® Tools/MSP-EXP430FR5969: Interface Board Flashing issue

Prodigy 50 points

Replies: 10

Views: 152

Part Number: MSP-EXP430FR5969

Tool/software: WEBENCH® Design Tools

Hi am Using Texas Instruments SmartRF Flash Programmer, connected it to IC M430FR5729 via JTag communication cable and the IC Is connected to 12V DC Supply, when I start to do flashing, the SmartRF Flash Programmer is showing that the device is unknown, But no other Application is actively using the MSP-FET, (Please take a look at the Attached Screen shot ) When i click on perform actions button the window is closing automatically

enter image description here

  • Hello,

    This programmer is mainly used to program the flash memory in Texas Instruments 8051-based low-power RF wireless MCUs, not the MSP430FR5729. A better option for your programming needs would be to use Uniflash. This programmer is always updated to support the latest devices from our product line.

    Best regards,

    Matt

  • In reply to umashankar bhukya:

    Hello,

    I went ahead and merged your latest posts with this thread because it is regarding the same exact issue. Please try to keep support for a specific topic local to the original thread so that a resolution is easily tracked.

    My answer is still the same as stated above:

    "This programmer is mainly used to program the flash memory in Texas Instruments 8051-based low-power RF wireless MCUs, not an MSP430FRxx device. A better option for your programming needs would be to use Uniflash. This programmer is always updated to support the latest devices from our product line."

    Best regards,

    Matt

  • Hello,

    Please refrain from making duplicate posts regarding the same issue. I am going to merge this post with the original thread.

    Best regards,

    Matt

  • In reply to Matt Calvo:

    Hey Matt,

    Thanks for reply

    Yes, Matt, I tried with UniFlash Programmer as well, when i put monitor device in AUTO, it is showing "No debug probes/devices detected". Please give me suggestions best way to do Flashing

    Setup using for flashing

    Screen Shot of UniFlash Programmer

    Best Regards

    Umashankar B

  • In reply to umashankar bhukya:

    Hello,

    The cause of the "No debug probes/devices detected" could be the result of an assortment of hardware/software issues. Could you please provide a schematic of the board you are trying to debug? From the picture you provided, it looks like the USB cable is frayed and that might be causing issues as well. You may want to try a new cable. You will also want to double check that the JTAG signals connected from the programmer to your board follow the recommended connections in the MSP430 Hardware Tools User's Guide (Figure 2-1, 2-2, or 2-3 depending on your project). 

    Best regards,

    Matt

  • In reply to umashankar bhukya:

    Hi Umashankar,

    Its been a couple of days since hearing from you. Have you been able to make any progress in your testing with regards to my previous comment?

    Best regards,

    Matt

  • In reply to Matt Calvo:

    Hi Umashankar,

    I am going to go ahead and mark this thread as "TI Thinks Resolved". If this is not the case please reply back with the status of your issue.

    Best regards,

    Matt