• TI Thinks Resolved

PMP10783: PMP10783 I don't really understand it

Prodigy 20 points

Replies: 2

Views: 50

Part Number: PMP10783

Hi TI
I am a newbie. I have a question . I do not understand this scheme. Can you help me explain?

  • Hi Do Van,

    The idea here is to use 400V rated capacitors (they are the most common and lowest cost in this range) to be able to support a higher input voltage.

    So we put the capacitors in series to increase the useable voltage.  The resistors are used to help balance the voltage on each cap.

    Hope this helps.

    Thanks,

    Robert

  • In reply to Robert Taylor1:

    Thanks a lot !