Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
A buck chopper is modelled in TINA software with UCC28C43. Power rating is 2.5kW. It has to operate from 65% duty to 96% duty @ 80 Hz. Model is successfully built to the requirements. Slope compensation parameters are calculated based on datasheet.
However, while testing the proto, results are not replicated to the simulation. We got sub-harmonic instability in the PWM output. We tried tuning every value of slope compensation parameters, didn't work. Current sensing is placed in switch path in beginning, now it changed to inductor path. Still, same result.
Output voltage voltage is regulated to the set value, throught the duty range, and response is smooth. No overshoots, no Undershoots.
I hope some of you can propose some clues/solution.
Thanks
Ravi