This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] TIDA-01599: What are the benefits of using TPS27S100 in the implementation of safe torque off functionality in Variable Speed Drives?

Prodigy 720 points

Replies: 1

Views: 626

Part Number: TIDA-01599

What are the benefits of using TPS27S100 (Single-Channel High-Side Switch) in the implementation of safe torque off functionality in Variable Speed Drives?

  • TIDA-01599 is a TI Reference Design that implements safe torque off functionality in variable speed drives (per IEC61800-5-2). 

    TPS27S100, which is a Single-Channel High-Side Switch, is used to turn ON/OFF isolated IGBT gate driver supply for implementing safe torque off (STO). It offers the following benefits in this STO implementation:

      • Turn ON/FF signal compatible with LVCMOS/LVTTL logic
      • Option to limit and monitor the current drawn by the isolated IGBT gate driver supply. This helps in monitoring the health of the power supply as well as stuck high fault at the output.
      • Wide Operating Voltage of 3.5 V to 40 V supports controlling gate driver power supply, being powered from 5 – 24v± 20% . This provides enough safety margin on the voltage rating.

    For additional information about this topic, please refer to section 2.6 "System Design Theory" of the User Guide for TIDA-01599.

    You can also download the design files (BOM, Schematic, Gerber) for this reference design from the TIDA-01599 folder.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.