This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] TIDA-01622: What are the benefits of using UCC28780 in the implementation of USB Type-C power delivery, AC/DC adapter solution?

Prodigy 720 points

Replies: 1

Views: 844

Part Number: TIDA-01622

What are the benefits of using UCC28780 in the implementation of high efficiency, high power density USB Type-C power delivery, AC/DC adapter solution?

  • TIDA-01622 is a fully tested TI Reference Design for high efficiency, high power density, USB Type-C power delivery, AC/DC adapter solution with a wide input voltage range (85 - 265VAC) for laptop adapters and smartphone charger applications.

    UCC28780 is used as the key PWM controller, where its Adaptive Zero Voltage Switching (ZVS) and Burst Control are vitally important to realize the peak efficiency 94% and high power density 30W/in3, and also easily meet the stringent global efficiency standards DoE Level VI and EU CoC V5 Tier-2.

    For additional information about this topic, please refer to section 2.3 "System Design Theory" of the User Guide for TIDA-01622.

    You can also download the design files (BOM, Schematic, Gerber) for this reference design from the TIDA-01622 folder.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.