This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00254: Can I use other manufacture cameras instead of point grey camera?

Part Number: TIDA-00254

The reference design supply the cameras that can be used, which is point grey FlyCapture2 or Microsoft LifeCam Cinema.

Can I use other cameras instead of the two above cameras?

If the camera can be replaced, what's the requirements should be meeted?

Thanks,