This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TINA/Spice: Errors importing .LIB Spice model into Tina-TI

Intellectual 330 points

Replies: 2

Views: 65

Tool/software: TINA-TI or Spice Models

Hi,

I'm having difficulty importing a .lib file for a schottky diode I got from ROHM.  The model is unencrypted.  When trying to use the "New Macro Wizard" to import the model I get two error messages.  The first is a "Syntax Element" error.

After clicking "OK" on the first error message, this next one pops up.

I'm not sure what is going on.  I've imported the model file into LTSpice without any issues so I know the model file itself is good.  I'm not sure why Tina-TI is having difficulty with it.  Here is the contents of the .LIB file I have.

* DRSX101MM-30 D model
* Model Generated by ROHM
* All Rights Reserved
* Commercial Use or
* Resale Restricted
* Date: 2009/02/17
.MODEL DRSX101MM-30 D
+ IS=598.08E-9
+ N=.66808
+ RS=28.158E-3
+ IKF=10.167E-3
+ XTI=2
+ EG=.57
+ CJO=300.10E-12
+ M=.53965
+ VJ=.73769
+ ISR=10.432E-6
+ NR=1.4000
+ BV=30
+ TT=10.605E-9

Anyone have any thoughts?

Thanks in advance,

Shawn

  • Hi Shawn,

    I was able to import it by removing the "-" from DRSX101MM-30 as shown below:

    .SUBCKT DRS A B

    D1 A B  DRSX101MM30

    .MODEL DRSX101MM30 D
    + IS=598.08E-9
    + N=.66808
    + RS=28.158E-3
    + IKF=10.167E-3
    + XTI=2
    + EG=.57
    + CJO=300.10E-12
    + M=.53965
    + VJ=.73769
    + ISR=10.432E-6
    + NR=1.4000
    + BV=30
    + TT=10.605E-9

    .ENDS

    Herman

  • In reply to Herman Theodorus:

    Thanks!  That fixed it for me!

    Shawn

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.