Tool/software: TINA-TI or Spice Models
Hi,
Can you suggest me a way to design a cree LED in Tina-TI for its simulation purposes. The part number of LED is MHBAWT0F0BD265E.
When I was trying to design I came up with such parameters:
Saturation current : 0.1
peak Wavelength = 455nm
Energy gap = hc/lambda = 2.73eV
Max frwd current = 350mA
Typical frwd current = 180mA
Max Power distribution = 7W
Now if I try to find serial resistance, since cree led does not have a linear graph of current versus voltage, I cannot find resistance. More importantly Cree led has current = 0 at 16V and 180mA at 18V. Therefore I don not need a linear graph. Thus even after changing emission coefficient, though threshold can be made 16V but linear graph is not changed and I am unable to get 180mA at 18V.
Can you please help?
Thanks in advance.cree_at_forum.TSC