Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
Could you please provide an unencrypted PSPICE or SPICE3f5 model of the LMG1020? I can sign an NDA to avoid public disclosure of this IP, and you can email it to me directly.
The problem I have is I am modeling a circuit that uses the LMG1020 using the Altium Designer-based Circuit Simulator (Altium Designer v19). The Simulator uses an enhanced version of the event-driven XSpice, developed by the Georgia Tech Research Institute (GTRI), which itself is based on Berkeley's SPICE3 code. It is fully SPICE3f5 compatible, as well as providing support for a range of PSpice® device models.
Reference (Find, "SPICE3f5 compatible"):
It seems that Altium cannot handle encrypted PSPICE modles. Also some PSPICE models require conversion in order to be used with the Altium Designer Simulator. I cannot do this when the model is encrypted.
Reference (Find, "currently not supported")
techdocs.altium.com/.../Linking a Simulation Model to a Schematic Component