This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TIDA-00067: Simulation, hardware & system design tools forum

Prodigy 10 points

Replies: 1

Views: 161

Part Number: TIDA-00067

Hi,

We are intended to prove PLC communication between devices which is currenty RS 485 active on them.

I am looking for;

1) PLC on 48 VDC, but the DC will be changing 40V to 60V

2) Bit rate is 115200.

3) Transmission distance is about 0,6 meter.

4) Support UART input and UART output. That is, UART to PLC or PLC to UART.

I need suggestions and software information in order to start my work.

BR/Arslan

  • Hi,

    Please take a look at TIDA-060001.  Hardware files are given and software is open-source which will allow you get started quickly.

    Gus Martinez

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.