As suggested, the R58 connection was moved to VDD Node & Changed the total resistor value of R38+R40+R42+R43+R45+R46 to 15K to enable the Self start up to avoid connecting the +20V & -5V externally. However this didn't work. Could you please suggest if there are any additional changes required to facilitate the self startup? If there any reduction envisaged in the resistor network ( R37,....,R49 ) from 9MOhm to a lower value to increase the base current of Q9?